Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
Software & Development Tools
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Software & Development Tools
  • Processors & DSP
Software & Development Tools
Documents How to use assembly function in C++ code
  • Q&A
  • Documents
  • Members
  • Tags
  • Cancel
  • -Documents
    • -Software and Development Tools
      • BSP package and Help page for Linux
      • Does CCES supports argc and argv in ARM?
      • -How to use assembly function in C++ code
        • Calling assembly function from C code
      • I have a purchase/order details, but lost the license key. What should I do to get my purchased license key?
      • Inline ASM code using scratch register
      • L1 Block2 PM in Sharc+ core
      • Legacy SHARC to SHARC+ migration
      • Refresh memory window at runtime
  • +ADSP-SC58x: FAQ
  • +Blackfin BF707: FAQ
  • +CCE: FAQ
  • +CCES 2.6.0: FAQ
  • +CCES 2.8.0: FAQ
  • +External identifier in assembler: FAQ
  • +GCC Compiler Manual: FAQ
  • +VisualDSP++: FAQ

How to use assembly function in C++ code

Question:
How to use assembly function in C++ code?

Answer:
When using asm code from C++ code, you have to inform the build tools that these functions are in asm, so that it knows how to call them. When a asm source file is compiled, the function names are given an underscore prefix in the generated assembly. For example, "void foo(int a) {...}" becomes "_foo" in the generated assembly. This is the symbol used to call the function.

As C++ supports function overloading, simply adding an underscore would not differentiate between the variances of the same function. So, a suffix is added to the symbol name in assembly when a C++ source file is compiled. For example. "void foo(void)" becomes "_foo__Fv" ("__F" = function, "v" = void), while "void foo(unsigned char *a, int b)" would become "_func__FPUci" in the assembly file, where the "__FPUci" means the Function ("__F") takes a Pointer ("P") to an Unsigned char ("Uc"), and an integer ("i") as it's parameters: "__FPUci".

This is true not only when you build the source that contains the function definition, but also when you call the function from your code. Where this causes problems, is if you call "foo(void)" from your C++ source, but the function exists in a asm source file, the generated assembly will call "_foo_Fv", but the linker will not be able to resolve that reference, as compiling the C source file would only produce a symbol "_foo".

You can let the Compiler know how to resolve these references using the "extern" qualifier. For example, if you have a function named "asm_func()" in a asm source file, simply add the prototype to your C++ source code (or a header file included by the C++ source) as follows:

extern "asm" void asm_func(void);

This tells the C++ Compiler that "asm_func ()" is a asm function, and will generate references to this function in the generated assembly.

Also please note that, no need to add dot suffix in function definition of " asm_func()”, while using extern qualifier.