Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Calibration Implementation Techniques for Multichannel Phased Array Subsystems

    Learn about phase-calibration techniques used for characterizing a 16 transmit and 16 receive X-band phased array subsystem based on a mixed-signal front...

EngineerZone
EngineerZone
VisualDSP++ Development Tools
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
VisualDSP++ Development Tools
  • Processors & DSP
  • Software & Development Tools
  • VisualDSP++ Development Tools
  • Cancel
VisualDSP++ Development Tools
Documents A number of registers appear to be missing from sysreg.h in VisualDSP++ 5.0 compared to earlier versions
  • Q&A
  • Documents
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADSP-21369 EZ-KIT: FAQ
  • +ADSP-BF506F: FAQ
  • +ADSP-BF592: FAQ
  • +Blackfin: FAQ
  • +DXE: FAQ
  • +How to Resolve [Error li1040]: FAQ
  • +HP-USB-ICE Emulator: FAQ
  • +ICE1000: FAQ
  • Is it possible to convert my existing floating license to node-locked license or vice versa?
  • +Project Building Error: FAQ
  • +Reset, Reload and Restart: FAQ
  • +SHARC simulator: FAQ
  • Ticks for VDK_Sleep()
  • +VDK heap: FAQ
  • -VisualDSP++: FAQ
    • A number of registers appear to be missing from sysreg.h in VisualDSP++ 5.0 compared to earlier versions
    • Able to install the base release of VisualDSP++ 5.0 without any problems but encountering a 'Could not find XML file or the XML file might be corrupted!’ message when trying to install an update. Audit
    • Advantages of using 'Run as Administrator' on Windows 7 or 8 for VisualDSP++
    • After reformatting my hard-drive and reinstalling VisualDSP I get the error "A valid license could not be found" error, and can no longer run VisualDSP.
    • Are international character sets supported by VisualDSP++?
    • Can I install your Floating License Tools on a server running Linux?
    • Can I run more than one instance of VisualDSP++ at a time?
    • Can I undo a VisualDSP++ Update or roll-back to a previous update?
    • Can we create the FPGA program with VisualDSP?
    • Compile VDSP project using make file
    • corrupt project file Error VisualDSP++ 3.0
    • Does VisualDSP++ include a Stand Alone Flash Programmer?
    • Does VisualDSP++ use absolute or relative paths?
    • Does VisualDSP++®︎ support the new ADSP-BF60x processor family? Audit
    • Error "The XML page cannot be displayed" when trying to view a linker map file
    • Error Connecting to ADSP-21489 EZ-Kit Visual DSP++
    • ftell function return value in VDSP
    • Guidelines for Posting VisualDSP++ Development Tools Issues
    • How can I obtain 90 days test drive license for VisualDSP++?
    • How can I obtain the VisualDSP++ Software License Agreement?
    • How can I obtain university license for VDSP?
    • How can I specify different compiler options for individual files in a project?
    • How can you use a C-function, defined in a separate file, in a method of a C++-class?
    • How do I configure my Firewall for a Floating License
    • How do I Enable Python script in VDSP
    • How do I move my VisualDSP++ Floating License Server to a new machine?
    • How do I use FLEXnet Licensing with more than one product? Can I combine license.dat files? Audit
    • How do I verify the Analog Devices products, versions and licenses that are installed on my computer?
    • How do you view a Map file? Audit
    • How does the IDDE know which words to syntax highlight?  Can I add my own words to this list?
    • How to build .bin in VisualDSP++
    • How to generate a makefile from a VisualDSP++ project?
    • How to generate assembly code (.s files) from Visual DSP project?
    • How to load and run a program from flash on an EZ-KIT in VisualDSP++?
    • How to run Stand-Alone Flash Programmer without VisualDSP++ environment?
    • How to transfer VisualDSP++ Floating License Server to new machine?
    • How to use License Borrowing feature of VisualDSP++
    • How to use relative paths in VisualDSP?
    • How to use the function of image processing toolbox with Visual DSP++? Audit
    • How to Verify Contents of Flash using VisualDSP++?
    • I am looking for the source files of runtime libraries which is provided by VisualDSP++ Tools. Where I can find them?
    • I have installed a Test Drive license. Why can't I create an "EZ-KIT Lite" session?
    • I need to transfer my license to a new machine (or, my hard drive crashed and had to be reformatted). How do I register my license against a new host ID? Audit
    • I uninstalled VisualDSP++ due to a problem, and now when I’m trying to reinstall my serial number I receive the message “The serial number has already been used and can be installed only once”. What should I do?
    • I've recently upgraded to VisualDSP++ 5.0 from VisualDSP++ 3.5 or earlier. My license.dat file was copied over during installation, but only Simulator sessions are now available.
    • In VDSP, can we switch between DHCP and static IP at run time Audit
    • Installation error “Error registering a file with Windows” for VDSP++ in windows 10
    • Installation Failure error in VDSP while calling 21020ICE.inf file
    • Is it possible to accept third party agreement for supporting VDSP on Windows 10
    • Is it possible to backup/restore a VisualDSP++ Session
    • Is it possible to mix objects produced by different versions of VisualDSP++?
    • Is the Green Hills Blackfin Processor development suite going to replace the VisualDSP++ suite?
    • Is there any tool in the Visual DSP that can monitor the thread occupied time?
    • I’ve just installed a full license or evaluation license and now I get a message telling me that the license will expire in X days. Audit
    • Placement of data in VisualDSP 3.5
    • Purpose of GetThreadStackUsage() function in VDSP toolchain?
    • Speeding up slow build times in VisualDSP++
    • Support for Parallel Builds in VisualDSP++
    • System requirements for VisualDSP++ and supported operating systems
    • The VisualDSP++ SAFP does not work on 64-bit machine's
    • Transforming source code asm21k .asm and .arch file from DSP21k Toolkit to VDSP 5.X.X?
    • Unable to enter breakpoints in my code in VisualDSP++.
    • Unable to view variables in the Locals window and the Expressions window displays "Expressions Window: ERROR: Unknown variable or symbol"
    • VDSP Installation via command prompt
    • VDSP license update inquiry
    • VDSP++ doesn't show file extension into editor tabs
    • Visual DSP++ runtime error
    • VisualDSP++ 5.0 SD card driver reports incorrect size/ fails to be recognized by Windows
    • VisualDSP++ 5.1.1 Download
    • VisualDSP++ 5.1.1 users should upgrade to VisualDSP++ 5.1.2
    • VisualDSP++ and 64-bit Windows
    • VISUALDSP++ DEVELOPMENT TOOLS
    • VisualDSP++ STDIO is slow, and interrupts processing of real-world data
    • What are the differences between the Compiled Simulator and the Cycle Accurate Simulator?
    • What are the different types of licenses for VisualDSP++?
    • What is the usage of optimization pragmas in VisualDSP? Audit
    • What OS will VisualDsp run under.
    • What types does VisualDSP++ compiler use to implement enumerations and enumeration constants? Audit
    • What's New in VisualDSP++ 5.0 Update 9? Audit
    • When I try to connect to VisualDSP++ via remote desktop I encounter the following error message - ERROR: Terminal Server remote client not allowed
    • When I try to install VisualDSP++ 5.0 on my Windows 7 machine I encounter a message stating that “Windows can’t verify the publisher of this driver software”. Why?
    • When I try to start VisualDSP++ 5.0 either from the Start menu or from within the System folder nothing happens.
    • When trying to install VisualDSP++ I encounter a number of errors, such as, 'Install cannot proceed. Could not find XML file or the XML file may be corrupted'. How do i resolve this? Audit
    • Where can I find details of Tools Anomaly Reports relating to VisualDSP++? Audit
    • Where is the C source file which defines VDK functions such as CreateThread() in VisualDSP++?
    • Where is the header file that defines VDK data types such as VDK_ThreadCreationBlock?
    • Where to find out how much memory is used in Visual DSP++ for Blackfin?
    • Which versions of VisualDSP++ are supported on Windows Vista?
    • Which VisualDSP++ Updates do I need to install?
    • Why do I receive, "The serial number has already been used and can be installed only once" when entering a Test Drive license?
    • Why does my code stop working when I enable optimization? Audit
    • Why does my LDF file not open in the Expert Linker in VisualDSP++ 5.0 Update 2?
    • Why is my Blackfin LDF marked as Read Only and why cant i make modifications to the text version of the file?
    • Will my License number work with different versions of VisualDSP?
    • Windows 7 Compatibility in VisualDSP++ Development Tools
  • +Windows 8.1: FAQ

A number of registers appear to be missing from sysreg.h in VisualDSP++ 5.0 compared to earlier versions

Q: A number of registers appear to be missing from sysreg.h in VisualDSP++ 5.0 is this correct? If so, why?

---------------------------

A: Yes this is correct. A number of registers have been removed from sysreg.h in this version of the tools because these registers can be used by the compiler and so reading from or writing to these registers in regular "C" code could result in unexpected behaviour as you have no way of knowing what values they are going to hold.

The compiler assumes that all sysregs are registers that aren't otherwise used by the compiler. So, saying sysreg_write(reg_r3, x) and then y = sysreg_read(reg_r3) doesn't necessarily mean that x == y because the compiler might have used r3 in between them.

The only way to write to or read from these registers directly is to use inline assembly, though when writing your code you should take into account the factors mentioned above.

The registers affected are R0-R7, xR0-xr15, HR0-HR7, xHR0-xHR15, P0-P5, xP0-xP11, FP, SP and Q0-Q3.

Tags: visualdsp++ compiler