Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
VisualDSP++ Development Tools
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
VisualDSP++ Development Tools
  • Processors & DSP
  • Software & Development Tools
  • VisualDSP++ Development Tools
  • Cancel
VisualDSP++ Development Tools
Documents How to use License Borrowing feature of VisualDSP++
  • Q&A
  • Documents
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADSP-21369 EZ-KIT: FAQ
  • +ADSP-BF506F: FAQ
  • +ADSP-BF592: FAQ
  • +Blackfin: FAQ
  • +DXE: FAQ
  • +How to Resolve [Error li1040]: FAQ
  • +HP-USB-ICE Emulator: FAQ
  • +ICE1000: FAQ
  • Is it possible to convert my existing floating license to node-locked license or vice versa?
  • +Project Building Error: FAQ
  • +Reset, Reload and Restart: FAQ
  • +SHARC simulator: FAQ
  • Ticks for VDK_Sleep()
  • +VDK heap: FAQ
  • -VisualDSP++: FAQ
    • A number of registers appear to be missing from sysreg.h in VisualDSP++ 5.0 compared to earlier versions
    • Able to install the base release of VisualDSP++ 5.0 without any problems but encountering a 'Could not find XML file or the XML file might be corrupted!’ message when trying to install an update. Audit
    • Advantages of using 'Run as Administrator' on Windows 7 or 8 for VisualDSP++
    • After reformatting my hard-drive and reinstalling VisualDSP I get the error "A valid license could not be found" error, and can no longer run VisualDSP.
    • Are international character sets supported by VisualDSP++?
    • Can I install your Floating License Tools on a server running Linux?
    • Can I run more than one instance of VisualDSP++ at a time?
    • Can I undo a VisualDSP++ Update or roll-back to a previous update?
    • Can we create the FPGA program with VisualDSP?
    • Compile VDSP project using make file
    • corrupt project file Error VisualDSP++ 3.0
    • Does VisualDSP++ include a Stand Alone Flash Programmer?
    • Does VisualDSP++ use absolute or relative paths?
    • Does VisualDSP++®︎ support the new ADSP-BF60x processor family? Audit
    • Error "The XML page cannot be displayed" when trying to view a linker map file
    • Error Connecting to ADSP-21489 EZ-Kit Visual DSP++
    • ftell function return value in VDSP
    • Guidelines for Posting VisualDSP++ Development Tools Issues
    • How can I obtain 90 days test drive license for VisualDSP++?
    • How can I obtain the VisualDSP++ Software License Agreement?
    • How can I obtain university license for VDSP?
    • How can I specify different compiler options for individual files in a project?
    • How can you use a C-function, defined in a separate file, in a method of a C++-class?
    • How do I configure my Firewall for a Floating License
    • How do I Enable Python script in VDSP
    • How do I move my VisualDSP++ Floating License Server to a new machine?
    • How do I use FLEXnet Licensing with more than one product? Can I combine license.dat files? Audit
    • How do I verify the Analog Devices products, versions and licenses that are installed on my computer?
    • How do you view a Map file? Audit
    • How does the IDDE know which words to syntax highlight?  Can I add my own words to this list?
    • How to build .bin in VisualDSP++
    • How to generate a makefile from a VisualDSP++ project?
    • How to generate assembly code (.s files) from Visual DSP project?
    • How to load and run a program from flash on an EZ-KIT in VisualDSP++?
    • How to run Stand-Alone Flash Programmer without VisualDSP++ environment?
    • How to transfer VisualDSP++ Floating License Server to new machine?
    • How to use License Borrowing feature of VisualDSP++
    • How to use relative paths in VisualDSP?
    • How to use the function of image processing toolbox with Visual DSP++? Audit
    • How to Verify Contents of Flash using VisualDSP++?
    • I am looking for the source files of runtime libraries which is provided by VisualDSP++ Tools. Where I can find them?
    • I have installed a Test Drive license. Why can't I create an "EZ-KIT Lite" session?
    • I need to transfer my license to a new machine (or, my hard drive crashed and had to be reformatted). How do I register my license against a new host ID? Audit
    • I uninstalled VisualDSP++ due to a problem, and now when I’m trying to reinstall my serial number I receive the message “The serial number has already been used and can be installed only once”. What should I do?
    • I've recently upgraded to VisualDSP++ 5.0 from VisualDSP++ 3.5 or earlier. My license.dat file was copied over during installation, but only Simulator sessions are now available.
    • In VDSP, can we switch between DHCP and static IP at run time Audit
    • Installation error “Error registering a file with Windows” for VDSP++ in windows 10
    • Installation Failure error in VDSP while calling 21020ICE.inf file
    • Is it possible to accept third party agreement for supporting VDSP on Windows 10
    • Is it possible to backup/restore a VisualDSP++ Session
    • Is it possible to mix objects produced by different versions of VisualDSP++?
    • Is the Green Hills Blackfin Processor development suite going to replace the VisualDSP++ suite?
    • Is there any tool in the Visual DSP that can monitor the thread occupied time?
    • I’ve just installed a full license or evaluation license and now I get a message telling me that the license will expire in X days. Audit
    • Placement of data in VisualDSP 3.5
    • Purpose of GetThreadStackUsage() function in VDSP toolchain?
    • Speeding up slow build times in VisualDSP++
    • Support for Parallel Builds in VisualDSP++
    • System requirements for VisualDSP++ and supported operating systems
    • The VisualDSP++ SAFP does not work on 64-bit machine's
    • Transforming source code asm21k .asm and .arch file from DSP21k Toolkit to VDSP 5.X.X?
    • Unable to enter breakpoints in my code in VisualDSP++.
    • Unable to view variables in the Locals window and the Expressions window displays "Expressions Window: ERROR: Unknown variable or symbol"
    • VDSP Installation via command prompt
    • VDSP license update inquiry
    • VDSP++ doesn't show file extension into editor tabs
    • Visual DSP++ runtime error
    • VisualDSP++ 5.0 SD card driver reports incorrect size/ fails to be recognized by Windows
    • VisualDSP++ 5.1.1 Download
    • VisualDSP++ 5.1.1 users should upgrade to VisualDSP++ 5.1.2
    • VisualDSP++ and 64-bit Windows
    • VISUALDSP++ DEVELOPMENT TOOLS
    • VisualDSP++ STDIO is slow, and interrupts processing of real-world data
    • What are the differences between the Compiled Simulator and the Cycle Accurate Simulator?
    • What are the different types of licenses for VisualDSP++?
    • What is the usage of optimization pragmas in VisualDSP? Audit
    • What OS will VisualDsp run under.
    • What types does VisualDSP++ compiler use to implement enumerations and enumeration constants? Audit
    • What's New in VisualDSP++ 5.0 Update 9? Audit
    • When I try to connect to VisualDSP++ via remote desktop I encounter the following error message - ERROR: Terminal Server remote client not allowed
    • When I try to install VisualDSP++ 5.0 on my Windows 7 machine I encounter a message stating that “Windows can’t verify the publisher of this driver software”. Why?
    • When I try to start VisualDSP++ 5.0 either from the Start menu or from within the System folder nothing happens.
    • When trying to install VisualDSP++ I encounter a number of errors, such as, 'Install cannot proceed. Could not find XML file or the XML file may be corrupted'. How do i resolve this? Audit
    • Where can I find details of Tools Anomaly Reports relating to VisualDSP++? Audit
    • Where is the C source file which defines VDK functions such as CreateThread() in VisualDSP++?
    • Where is the header file that defines VDK data types such as VDK_ThreadCreationBlock?
    • Where to find out how much memory is used in Visual DSP++ for Blackfin?
    • Which versions of VisualDSP++ are supported on Windows Vista?
    • Which VisualDSP++ Updates do I need to install?
    • Why do I receive, "The serial number has already been used and can be installed only once" when entering a Test Drive license?
    • Why does my code stop working when I enable optimization? Audit
    • Why does my LDF file not open in the Expert Linker in VisualDSP++ 5.0 Update 2?
    • Why is my Blackfin LDF marked as Read Only and why cant i make modifications to the text version of the file?
    • Will my License number work with different versions of VisualDSP?
    • Windows 7 Compatibility in VisualDSP++ Development Tools
  • +Windows 8.1: FAQ

How to use License Borrowing feature of VisualDSP++

Q:

I am looking for detailed instructions for using new License Borrowing feature in VisualDSP++ 5.0.

--------------------------------------------

A:

The licenses can be checked out either by using the lmborrow.exe (command-line) tool, or using the LMTOOLS application (GUI) , and can be borrowed up to a maximum of 30 days.

Using the LMTOOLS GUI

If you would rather use a GUI interface to borrow licenses, check the status, return licenses early or stop license borrowing, you can use the LMTOOLS application. LMTOOLS can be found in the same folder the lmborrow utility is located on the license server. To use LMTOOLS, you will need to copy the application to your client system.

To borrow licenses with LMTOOLS, start the application and click on the "Borrowing" tab.  In the Vendor Name field type in "analogd."  In the Return Date enter the date the licenses are to be borrowed until and for the Return Time field enter the time to return the licenses (24 hour format). Then click the "Set Borrow Expiration" button.

To actually borrow the licenses for the various features (VDSP-DEBUGGER, SIMULATOR-FRIO, COMPILER-FRIO, etc.) you need to start VisualDSP++ and build a program that targets the processor type you are developing for. By doing that all the necessary licenses will be borrowed so you can do your development while disconnected from the server.

You can check the status of borrowed licenses with the LMTOOLS by starting the application and click on the "Borrowing" tab. Click the "List Currently Borrowed Features" button to see what licenses have been borrowed and when they are set to expire. You can also return borrowed licenses early using LMTOOLS. To do so you must first create an Environment variable called LM_LICENSE_FILE with a value of the path to the license file (default is C:\Program Files\Analog Devices\VisualDSP 5.0\System\license.dat). Then from the "Borrowing" tab, enter the name of the feature whose license is to be returned early in the Feature Name data field and click the "Return Borrowed Licenses Early" button to return the license for that feature. This has to be done for all features that are borrowed.

To stop borrowing licenses using LMTOOLS, start the application and click on the "Borrowing" tab. The user then just needs to click the "Don't Borrow Anymore Today" button to stop license borrowing.

Using the lmborrow.exe Command Line Interface
If you prefer to use the command-line application, "lmborrow.exe", to initiate license borrowing, check the status of borrowed licenses, return licenses before their expiration and stop borrowing licenses, you can do so by copying the "lmborrow.exe" to the client machine from the VisualDSP++ Floating License Server install at <install path>\LMSERVER.

The syntax to initiate license borrowing is:
    lmborrow analogd end_date [time]

where "analogd" is the name of the process running on the license server that serves the licenses and end_date is the date when the license will expire. The format for the end date component is dd-mmm-yyyy where dd is the day, mmm is the month (may, jun, jul, aug, etc.) and yyyy is the year. The optional time part is the time on the end date the license will expire.  The format for the time component is hh:mm where hh is the hour and mm is the minutes. It is in a 24 hour format.  Example: To borrow a license until June 15, 2008 at 1:00pm the user issues the following command from a DOS prompt:
    lmborrow analogd 15-jun-2008 13:00.

To actually borrow the licenses for the various features (VDSP-DEBUGGER, SIMULATOR-FRIO, COMPILER-FRIO, etc.) you need to start VisualDSP++ and build a program that targets the processor type you  are developing for. By doing that all the necessary licenses will be borrowed so you can do your development while disconnected from the server.

The syntax to check the status of borrowed licenses is: lmborrow -status. The command will give the following output (depending on the end date and time specified when borrowing the licenses):

    C:\FlexLM Command-line Apps>lmborrow -status

    lmborrow - Copyright (c) 1989-2005 Macrovision Europe Ltd. and/or Macrovision Corporation. All Rights Reserved.
    Vendor     Feature               Expiration
    ______     ________              __________
    analogd    VDSP-DEBUGGER         15-May-08 12:59
    analogd    EMULATOR-SHARC        15-May-08 12:59
    analogd    SIMULATOR-FRIO        15-May-08 12:59
    analogd    SIMULATOR-SHARC       15-May-08 12:59
    analogd    EMULATOR-FRIO         15-May-08 12:59
    analogd    EMULATOR-TIGERSHARC   15-May-08 12:59
    analogd    SIMULATOR-TIGERSHARC  15-May-08 12:59
    analogd    ASSEMBLER-FRIO        15-May-08 12:59
    analogd    LINKER-FRIO           15-May-08 12:59

The syntax to return licenses early is:  lmborrow -return -c "<path to license file>" <feature name>.  The -c option is optional but it is strongly recommended that you use it as lmborrow usually cannot find the license file without it. The path to the license file is the System folder in the install path specified when VisualDSP++ was installed. The default is "C:\Program Files\Analog Devices\VisualDSP 5.0\System\license.dat". The feature name is the same as the ones listed in the output from the lmborrow -status command.

The syntax to stop license borrowing is: lmborrow -clear. By running this command any more requests from the client to the server for a license will not result in that license being borrowed.

This FAQ was generated from the following discussion: How to use License Borrowing feature of VisualDSP++

Tags: visualdsp++ licensing floating
  • Share
  • History
  • More