Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    • Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    The Right Switch-Mode Power Supply Control Scheme

    This article compares three switch-mode power supply control schemescurrent-mode control, voltage-mode control, and hysteretic-mode control to guide engineers...

EngineerZone
EngineerZone
VisualDSP++ Development Tools
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
VisualDSP++ Development Tools
  • Processors & DSP
  • Software & Development Tools
  • VisualDSP++ Development Tools
  • Cancel
VisualDSP++ Development Tools
Documents Ticks for VDK_Sleep()
  • Q&A
  • Documents
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADSP-21369 EZ-KIT: FAQ
  • +ADSP-BF506F: FAQ
  • +ADSP-BF592: FAQ
  • +Blackfin: FAQ
  • +DXE: FAQ
  • +How to Resolve [Error li1040]: FAQ
  • +HP-USB-ICE Emulator: FAQ
  • +ICE1000: FAQ
  • Is it possible to convert my existing floating license to node-locked license or vice versa?
  • +Project Building Error: FAQ
  • +Reset, Reload and Restart: FAQ
  • +SHARC simulator: FAQ
  • Ticks for VDK_Sleep()
  • +VDK heap: FAQ
  • +VisualDSP++: FAQ
  • +Windows 8.1: FAQ

Ticks for VDK_Sleep()

Question:
What will happen when the number of ticks for VDK_Sleep() is set to 0, even if the minimum number of ticks allowed is 1?

Answer:
If an API is called from an inappropriate level, a KernelPanic is typically raised. For this VDK_Sleep(), the possible error code is "kInvalidDelay". We can see this details from the VDK status window( You can navigate via "View -> VDK Windows -> Status).

VDK calls an internal function named KernelPanic() under certain circumstances to indicate an error from which the system cannot recover. By default, the function loops indefinitely so that users can determine that a problem has occurred and provide information to facilitate debugging.
The KernelPanic() function disables interrupts on entry to ensure that execution loops in the intended location. We can override KernelPanic() in order to handle these types of errors differently; for example, you can reset the hardware when a KernelPanic occurs.
The circumstances under which KernelPanic() is called include the following.
• Errors in the creation of a VDK boot item during startup
• Runtime errors that are not handled by a C/C++ Thread’s error handler
• VDK internal errors

Refer "VDK Error Codes and Error Values" chapter in the 'VDK (Kernel) User’s Guide' from the below help page for more information on the possible errors for VDK API's:
Help > Contents > Manuals > Software Tools Manuals > VDK Manual > VDK (Kernel) User’s Guide > 5 VDK API Reference > VDK Error Codes and Error Values