Post Go back to editing

Project Building Error - An invalid argument was encountered

When building a project I encounter a dialog box with the following error:  "An invalid argument was encountered".  What's the cause of this error and how can I avoid it?

  • When adding files to your project, VisualDSP++ will use a relative path if the files are on the same drive as the project file. It will use an absolute path if the files are on a different drive to the project file.

    The only exception to this is if the file is located in the VisualDSP installation directory.  In this case, the install path is replaced with $VDSP.

    For example, if you are adding "C:\Program Files\Analog Devices\VisualDSP 5.0\Blackfin\Examples\Tutorial\dot_product_c\dotprod.c" into your project, dotprod.c is stored as "$VDSP\Blackfin\Examples\Tutorial\dot_product_c\dotprod.c" in the .dpj file.

    When adding paths to Project Options (such as include files) the decision is left to the user. When using the 'browse' functionality provided, an absolute path is added. If the user chooses to change that path to a relative one, it will remain so.

  • This question has been closed by the EZ team and is assumed answered.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.