Post Go back to editing

I can not connect to my ADSP 21062 with an ADZS-HPUSB-ICE

Hi there,

I am trying to connect to my dsp and is imposible to do. I am follo wing the manual:

The Sequence for Power On is:

1. Apply power to the target board.

2. Apply power to the ICE.

3. Connect the USB cable to the ICE.

4. Open the VisualDSP++ tools.

And when I click to connect(Visual DSP++ update 9.1) I obtain the error 0x 80048049. The connect light is amber as I attach to this message. I am pretty sure I have connected propperly all wires.

Thank you for your help

Parents
  • I have been testing the ICE with the VisualDsP++configurator and the test failed at the point of "Determining scan path length". In the documentation it is said that it could be a failure of my ICE but the most probably thing is that there is a problem with the target device. The fact is that I also have another ICE and with this one I dont have any type of problems with the same target. Is my ICE definitively damaged and it must be checked by qualified personnel???

Reply
  • I have been testing the ICE with the VisualDsP++configurator and the test failed at the point of "Determining scan path length". In the documentation it is said that it could be a failure of my ICE but the most probably thing is that there is a problem with the target device. The fact is that I also have another ICE and with this one I dont have any type of problems with the same target. Is my ICE definitively damaged and it must be checked by qualified personnel???

Children
No Data