Post Go back to editing

How to use rfft2d_fr16 or rfft2d_fr32 on grayscale images

Category: Software
Product Number: BF-609
Software Version: CCES 2.12.1

Hi,

I am trying to use rfft2d_fr16 function for FFT, but unaware of what size of images should i use for input buffers and output buffers and temp buffers. If you tell me it will be so helpful and i need sample input and output images to verify my result as per image viewer or array data if it is complex data.

Thanks,

Santhosh

  • Hi Santhosh,

    Thank you for your inquiry.

    You can get the detailed information about this library function and sample code from the below CCES help path

    CrossCore® Embedded Studio 2.12.0 > Blackfin® Development Tools Documentation > C/C++ Compiler and Library Manual for Blackfin® Processors > DSP Run-Time Library > DSP Run-Time Library Reference

    Hope this helps.

    Best Regards,
    Santhakumari.V

  • Hi Santhakumari,

    I worked on rfft2d_fr16() , to validate this I used it's FFT output as input to ifft2d_fr16(), for FFT size 64 , twiddle stride 1, block exponent 12, scale 1 , but I am getting 12 bits scaled while compared input see below

    1) My input is img[64*64 ]={0x7fff,0x7fff,0x7fff,0x7fff,0x7fff,.......0x7fff}

    ifft2d_fr16 output is ={0x7,0x7,0x7,0x7,.......0x7};

    2) My input is img[64*64 ]={0x4000,0x4000,0x4000,0x4000,........0x4000}

    Ifft2d_fr16 output is ={0x4,0x4,0x4,0x4,.......0x4};

    I changed my scaling values in both functions many times as well block exponent values also, but there is no change in ifft out.

    If changed FFT_SIZE to 32 or 16 then output occuring like 8, 6 bit scaling respectively, my question is while I am taking 64*64 input image, should i use only 64 FFT size or other FFT size.

    Another question is can i change my scaling factor .

    Thanks and regards,

    Santhosh