Post Go back to editing

ICE-1000 being recognized as ICE-100B

Category: Hardware
Product Number: ICE-1000
Software Version: Visual DSP++

I think my ICE-1000 has been impacted by the bug outlined in this ticket:

 ICE-1000/ICE-2000 detected as an ICE-100B after working with VisualDSP++ 5.1.1 

Has anyone successfully “recovered” their ICE-1000 after this?

Its showing up as an ICE-100B in device manager and I can’t now connect to my target.

I’ve tried manually updating the drivers, but that’s not helped.

Thanks and regards,

Mike

Parents
  • Hi,
     
    If you are facing this issue in VisulDSP++ 5.1.2, We recommend to try uninstall the emulator driver and reinstall the emulator driver manually once again using the below steps.

    The emulator driver  (WmUsbIce.sys for 32-Bit machines) and (WmUsbIce64.sys for 64-Bit machines) for the ADZS-ICE-1000 is located at the following path.
    ([install_drive]\ Program Files(x86)\Analog Devices\VisualDSP 5.x\Setup\Emu_Drivers)

    Please follow the below procedure for manually install driver:
    1.Go to Windows Device manager and uninstall the emulator driver by right clicking the emulator device.
    2.Go to Windows\system32\driver folder and delete the WmUsbIce.sys and WmUsbIce64.sys files.
    3.Go to Windows\inf folder (note this may be hidden) and search for files named "oem**.inf" and delete the files which contains the string "89982A59-5EEA-45aa-AF97-52EC351018C2" inside the file.These all of which are Analog Devices inf files, and must be deleted to ensure that your system does not pick up the existing drivers.
    4.Disconnect USB cable from the PC.
    5.Power down, then reboot the PC.
    6.Connect USB to PC.At this point Windows should detect the new hardware.
    7.Try installing the driver manually by browse to the location ..\Emu_Drivers.

    Please refer to the chapter "Verifying Driver Installation and Attaching to an Emulation Target" in the below manual.
    www.analog.com/.../ICE_emu_1000_2000_rev_manual.pdf

    Let us know how you gets on.

    Regards,
    Nishanthi.V

  • Hi Nishanthi,

    I'm still having some issues with this.  I can now get my PC to recognise the ICE-1000 correctly:

    If I fire up the Visual DSP++ Configurator, I can successfully establish and test the connection to my target using the ICE-1000.

    However, when I got into Visual DSP++ to start a new session, the option to select the ICE-1000 is not available.

    If I click on the Configurator button, it takes me to this screen:

    This doesn't list the Platform I created earlier using the Visual DSP++ Configurator.  If I select New, there is no ICE-1000 option to select:

    Are you able to assist me in setting up the ICE-1000 emulator correctly?

    Regards,

    Mike

Reply
  • Hi Nishanthi,

    I'm still having some issues with this.  I can now get my PC to recognise the ICE-1000 correctly:

    If I fire up the Visual DSP++ Configurator, I can successfully establish and test the connection to my target using the ICE-1000.

    However, when I got into Visual DSP++ to start a new session, the option to select the ICE-1000 is not available.

    If I click on the Configurator button, it takes me to this screen:

    This doesn't list the Platform I created earlier using the Visual DSP++ Configurator.  If I select New, there is no ICE-1000 option to select:

    Are you able to assist me in setting up the ICE-1000 emulator correctly?

    Regards,

    Mike

Children