Post Go back to editing

simple example on using UART interrupt to receive buffer from serial

Category: Software
Product Number: ADSP-BF592

Hi,

i would appreciate help in writing a simple test code to read data from UART in interrupt mode.

I am a newbe here.

I started with CharECHO_UART example and i was able to connect a terminal emulator (using a USB-DB9 cable). Then using Tera Term i sent a file

to my board and in DMA mode i was able to read all bytes i received.

Then i try something like:

static ADI_UART_HANDLE hDevice;

static void UARTCallback(void* pHandle, uint32_t u32Arg, void* pArg) {


printf("UART CALLBACK!!!!\n");
ADI_UART_HANDLE pDevice = (ADI_UART_HANDLE)pHandle;
ADI_UART_EVENT event = (ADI_UART_EVENT)u32Arg;
uint16_t *data = (uint16_t*)pArg;

printf("complete buffer:%s\n", ReceiveBuffer);

/*

here's the problem: my ReceiveBuffer contains only the last char sent from Termina Emulator

*/

}

int32_t main(void) {

// open UART in bidirectional interrupt mode mode

adi_uart_Open(UART_DEVICE_NUM, ADI_UART_DIR_BIDIRECTION, gUARTMemory_interrupt, ADI_UART_BIDIR_INT_MEMORY_SIZE, &hDevice);

adi_uart_SetBaudRate(hDevice, 115200u);

adi_uart_SetConfiguration(hDevice, ADI_UART_NO_PARITY, ADI_UART_ONE_STOPBIT, ADI_UART_WORDLEN_8BITS);

adi_uart_RegisterCallback(hDevice, UARTCallback, (void*)0);

adi_uart_SubmitRxBuffer(hDevice, ReceiveBuffer, 2);

adi_uart_EnableRx(hDevice, true);

while (true){

// do nothing

}

}

The problem is i only get the last character sent from terminal. I need to catch all chars sent from terminal

Each message sent from terminal may have different length so i need to process each received byte individually

I searched a lot and was not able to find a basic example that help me to build a simple program that read from UART in interrupt mode