Post Go back to editing

How to link a ".lib" or ".a" file?

I am trying to use a roll pitch sensor which comes with an external motion processing library. The motion processing driver comes pre-compiled for ARM core platforms and includes ".a" or ".lib" files to link to. I tried specifying it under "Project Options -> Link -> General -> Additional Options" like I do for the ".dlb" library files but I get the error:

visualdsp [Error li1032] 'third_party\IMU\mpl\libmpllib.lib' is not a valid input file.

I am using a Blackfin ADSP-BF537 and the roll/pitch sensor is an InvenSense MPU-9250 which I am trying link with the InvenSense Motion Driver 6.12. Is it possible to link to a library compiled for the ARM architecture on the Blackfin?

Parents Reply Children