Hi,
I am not able to connect ADSP BF533 EZ-KIT Lite board to PC using Visual DSP 5.1. The error is 80048015 (open device driver failed).
I have installed manually the USB driver and the OS indicated that it is working properly.
There is a new USB driver for windows 10 64 bits?
Thank you.
Hello,
Please find the attached Emulator driver.
Best regards,
Santha kumari.K
Go to Windows Device manager and uninstall the emulator driver from the CrossCore Tools.
>> Couldnt find it.
3.Go to Windows\inf folder (note this may be hidden) and search for files named "oem**.inf" and delete the files which contains the string "89982A59-5EEA-45aa-AF97-52EC351018C2" inside the file.These all of which are Analog Devices inf files, and must be deleted to ensure that your system does not pick up the existing drivers.
>> There are no files with this string in it... only OEMxx.inf...
Really need to make this work... Thanks
Go to Windows Device manager and uninstall the emulator driver from the CrossCore Tools.
>> Couldnt find it.
3.Go to Windows\inf folder (note this may be hidden) and search for files named "oem**.inf" and delete the files which contains the string "89982A59-5EEA-45aa-AF97-52EC351018C2" inside the file.These all of which are Analog Devices inf files, and must be deleted to ensure that your system does not pick up the existing drivers.
>> There are no files with this string in it... only OEMxx.inf...
Really need to make this work... Thanks