Hi,
I am not able to connect ADSP BF533 EZ-KIT Lite board to PC using Visual DSP 5.1. The error is 80048015 (open device driver failed).
I have installed manually the USB driver and the OS indicated that it is working properly.
There is a new USB driver for windows 10 64 bits?
Thank you.
Hello,
Please find the attached Emulator driver.
Best regards,
Santha kumari.K
Dear friend, I tried that. Not a chance to make it work on windows 10 V2004. Have you found another way to make it work as well? Thank you
Go to Windows Device manager and uninstall the emulator driver from the CrossCore Tools.
>> Couldnt find it.
3.Go to Windows\inf folder (note this may be hidden) and search for files named "oem**.inf" and delete the files which contains the string "89982A59-5EEA-45aa-AF97-52EC351018C2" inside the file.These all of which are Analog Devices inf files, and must be deleted to ensure that your system does not pick up the existing drivers.
>> There are no files with this string in it... only OEMxx.inf...
Really need to make this work... Thanks
Hi,
Could you please try to replace the above attached libusb-1.0.dll from the zip file to the below directories. Before replacing take a backup copy of the original "libusb-1.0.dll" file that already available in the directory and drop the new one and let us know how result of emulator connectivity.
For CCES : C:\Analog Devices\CrossCore Embedded Studio x.x.x\System
For VDSP : C:\Program Files (x86)\Analog Devices\VisualDSP 5.1.2\System
Regards,
Nishanthi.V