Article Can we create the FPGA program with VisualDSP?

Question:
Do you provide a software tool to generate the FPGA program? Can we create the FPGA program with VisualDSP?

Answer:
The FPGA program should be written using the Xilinx ISE Tools, as VisualDSP++ is not able to produce output which is directly writable to the FPGA.

Site Search

For more information, please refer to the below link.

FPGA and Processors Compatible Reference Designs | Analog Devices

Note that we provide an Image Converter Tool, which allows the user to create ASCII images using the Xilinx tools and then convert them to a format that is easy to add to a VisualDSP project.


This is located at "<installation path>\Analog Devices\VisualDSP++ x.x.x\Blackfin\Examples\FPGA EZ-EXTENDER\FPGAImageConverter".

The FPGA Programmer Driver, for writing an FPGA image to your FPGA Extender using the VisualDSP++ Flash Programmer Utility, can be found in
"<installation path>\Analog Devices\VisualDSP++ x.x.x\Blackfin\Examples\FPGA EZ-EXTENDER\".

Please take a look at the examples - and, particularly, the 'FPGA Extender Readme.txt' - for the FPGA EZ-Extender. This explains how to convert the output from the xilinx tools for programming through VisualDSP++.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.