Question:
Both client and the Sever is Windows 8.1 and i am getting the following error .
Before changing changing the server to Windows 8.1 it was running on XP and client on Windows 8.1 and there was no problem .
After changing the server to Windows 8.1 i am getting the following error .
There is no problem of using VDSP++ on Server when the LM Tool is running , but cannot client side we are getting this error .
Tried with turning of the Firewall setting also but not able to get it working , please let me know if there any place to look for .
-----------------------------
Answer:
Unfortunately Floating licenses are not supported on windows 8.1. please note that our latest version of the Floating License Server Tools are supported on the following 32-bit operating systems:
• Windows 2000 SP4
• Windows XP Professional SP2 (or greater)
• Windows Vista Business/Enterprise/Ultimate
• Windows Server 2003
• Windows 7 Enterprise/Ultimate
And the following 64-bit operating systems:
• Windows 7 Enterprise/Ultimate.
This document was generated from the following discussion: With regards Floating License on Windows 8.1