EVAL-ADXL345Z-DB ARM C/C++ Compiler Issue

Dear Analog Support:

    I was so excited about getting the EVAL-ADXL345Z-DB as it had just about everything I needed to prototype a product that I am developing. However, when I launched the Keil uVision IDE Tool I get the following error:

"The ARM (t)c/c++ Compiler has encountered a problem and needs to close.  We are sorry for the inconvenience."

Then I am asked the usual prompt of do I want to send a report to Microsoft or not. I am not sure where the report would go other than an informational blackhole. After uninstalling and re-installing the Keil tool for the EVAL-ADXL345Z-DB platform, the issue still persisted. I am running on Windows XP, but is there a separate step to install the C/C++ compiler or is there something else that I should try other than uninstalling and re-installing the tool?

   I am able to download code to this nice Dev Board using the "uploader" tool.

Regards,


Manny

Parents
  • Manny, I am having a similar issue with this board. I need to work with the accelerometer but I cannot get the source file for the board to compile and so I am stopped unless someone can explain why it doesn't compile if it is the source of the DB? I don't think it is I get constant errors.  I can tell you this if you are using Keil's new release it will not work without the legacy upgrade because it does not support series 7 processors.  my problem is compiling errors so they are trying to help me understand the issue but need the attention of the product team. I am sort of in limbo.

    ken

Reply
  • Manny, I am having a similar issue with this board. I need to work with the accelerometer but I cannot get the source file for the board to compile and so I am stopped unless someone can explain why it doesn't compile if it is the source of the DB? I don't think it is I get constant errors.  I can tell you this if you are using Keil's new release it will not work without the legacy upgrade because it does not support series 7 processors.  my problem is compiling errors so they are trying to help me understand the issue but need the attention of the product team. I am sort of in limbo.

    ken

Children
No Data