H.264 codec in blackfin??

1) Is it possible implement both H.264 encoder and decoder in the same blackfin.

2) I have ADSP-BF527 EZ-KIT Lite, would I be able to compress live BT.656 format video input, so that the output rate should be less than 3.5Mbps.

     BT.656 format input is obtained using A-V EZ-Extender daughter card ( ADZS-BFAV-EZEXT  ) to which input is analog composite video.

3) What is the maximum resolution supported by BF527.

4) How to achieve HD or video resolution higher than D1 resolution video compression using H.264 BP encoder.

Kindly reply to this queries ASAP.

Regards,

Sunil

Parents
  • Hi,

    I am getting composite PAL analog video signal, digitized using ADV7183 whose output is in BT.656 format. I need to compress it to 4mbps using H.264 codec.

    This compressed data is decompressed using H.264 codec at other end and converted to analog signal using ADV7390.

    Frame rate = 25 Frames per second

    Bit rate = 27Mega Bytes per second ( BT.656 )

    Resolution = 720*480 ( PAL )

    Regards,

    Sunil

Reply
  • Hi,

    I am getting composite PAL analog video signal, digitized using ADV7183 whose output is in BT.656 format. I need to compress it to 4mbps using H.264 codec.

    This compressed data is decompressed using H.264 codec at other end and converted to analog signal using ADV7390.

    Frame rate = 25 Frames per second

    Bit rate = 27Mega Bytes per second ( BT.656 )

    Resolution = 720*480 ( PAL )

    Regards,

    Sunil

Children
No Data