Q.Does SigmaStudio for SHARC have any facility for working with multi-processor designs?
--------------------------------------
A.
This not fully supported at present. However, SigmaStudio can work with multiple instances in a single target in which the inter-instance communication is coordinated through the Application. For example, output audio from one instance can be fed to the next through application API interface buffers. Please refer to Annexure –B of the SigmaStudio_for_SHARC_ReferenceGuide.pdf for details on how to create a multi-instance Application