Q: Is it possible to generate target application LDR file with schematic 'code' and 'parameter' embedded in it?
---------------------------------------------------------------------------------------------------------------------------------------------
A: It is possible to create an application LDR file with schematic 'code' and 'parameter' embedded in it. Please refer to the attached document "SigmaStudio_No_Download_Mode.pdf" for more details.
Once this LDR file is booted on to the target, the schematic processing starts. There is no need to perform 'Link-Compile-Download' from the SigmaStudio host.
Alternately this LDR can be written to the target flash. This enables the user to boot the application from the flash and work without the USB to SPI conversion hardware.
* app.c inside ss4sharc_no_download.zip is based on SigmaStudio for SHARC 2.2.0