Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
SigmaStudio for SHARC
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
SigmaStudio for SHARC
  • Processors & DSP
  • Software & Development Tools
  • SigmaStudio for SHARC
  • Cancel
SigmaStudio for SHARC
Documents Integrating Additional Input/Output SPORT Interfaces in the ADSP-2156x Library Example
  • Q&A
  • Documents
  • Members
  • Tags
  • Cancel
  • +How the SigmaStudio schematic source files generated for DemoUc example application in SigmaStudio for SHARC 4.x.x version?
  • -SigmaStudio for SHARC: FAQ
    • ADSP-2156x Lib Integration Example as DemouC Application
    • ADSP-215xx/ADSP-SC5xx SigmaStudio For SHARC schematic custom plug-in debugging technique
    • Can I evaluate SigmaStudio for SHARC?
    • Can I rebuild Software Module Plug-In Loader files, originally built using SigmaStudio for SHARC 2.0.0, using SigmaStudio for SHARC 2.1.0?
    • Can I rebuild Software Module Plug-In Loader files, originally built using SigmaStudio for SHARC 2.0.0, using SigmaStudio for SHARC 2.2.0?
    • Can I use SigmaStudio for SHARC without a valid CrossCore Embedded Studio license?
    • Can I write my own custom modules for SigmaStudio?
    • Do you offer SigmaStudio for SHARC compatible Software Modules?
    • Does SigmaStudio for SHARC have any facility for working with multi-processor designs?
    • Does SigmaStudio for SHARC only work with the EZKits? Can I use it directly with my own product board?
    • How can I communicate with my SHARC evaluation or custom board using SigmaStudio for SHARC?
    • Integrating Additional Input/Output SPORT Interfaces in the ADSP-2156x Library Example
    • Is it possible to generate an application LDR with schematic code and parameter embedded in it?
    • SigmaStudio is free of charge. Is the same true for SigmaStudio for SHARC?
    • SigmaStudio™︎ for SHARC®︎ 2.2.0 – Getting Started
    • What algorithms are available for SigmaStudio for SHARC?
    • What is the difference between the USBI2EZB and the ADUSB2EBZ?
    • Which operating systems is SigmaStudio for SHARC supported on?
    • Why does SigmaStudio throw this message when a Schematic containing Plug-In modules is compiled?
    • Why does the Plug-In function as Production version even after uninstalling the Production version of the module installer?
    • Why is the macro NUM_SAMPLES missing in the Application?
    • Why is the SigmaStudio for SHARC installation failing?
    • Why there is no Audio output after my Schematic is downloaded?

Integrating Additional Input/Output SPORT Interfaces in the ADSP-2156x Library Example

Please find the documentation and examples which will help for Integrating Additional Input/Output SPORT Interfaces in the ADSP-2156x Library Example.

ADSP-21569.zip

  • Share
  • History
  • More