1.As seen in the picture, no compression is being applied yet.

2.After I set the compression threshold to about -15 dB, the output signal is clearly being limited when I compare it to the input.

3.When I turn up the input by 1 dB, the output goes up by 1 dB as well.

4.When I raise the input by 2 dB, the output actually drops by 1 dB.

5.From then on, each 1 dB input boost gives me 1 dB more output. But every time the input goes up by 3 dB, the output suddenly crashes down to my set threshold.



What's going on here? I don't see this problem with the RMS Compressor, and the Peak Compressor on the ADAU1466 doesn't behave like this either—it stays stable the whole time.