Post Go back to editing

The Peak Compressor in SigmaStudio+ behaves unstably when compressing signals on the ADSP-21565.

Thread Summary

The user reported an issue with the Peak Compressor in SigmaStudio+ where the output signal drops unexpectedly when the input is increased beyond a certain threshold, unlike the stable behavior in the RMS Compressor and the Peak Compressor on the ADAU1466. The issue has been confirmed and is planned for a fix in the v3.5.0 release. The user used a 1 kHz sine wave for testing and confirmed the input signal stability, suggesting the problem lies in the compressor's internal gain calculation logic.
AI Generated Content
Category: Software
Product Number: adsp-21565
Software Version: sigma studio+ 3.4.0

1.As seen in the picture, no compression is being applied yet.

2.After I set the compression threshold to about -15 dB, the output signal is clearly being limited when I compare it to the input.

3.When I turn up the input by 1 dB, the output goes up by 1 dB as well.

4.When I raise the input by 2 dB, the output actually drops by 1 dB.

5.From then on, each 1 dB input boost gives me 1 dB more output. But every time the input goes up by 3 dB, the output suddenly crashes down to my set threshold.

What's going on here? I don't see this problem with the RMS Compressor, and the Peak Compressor on the ADAU1466 doesn't behave like this either—it stays stable the whole time.

Thread Notes

  • Hi,

    Thank you for your patience, and we apologize for the delay. This case was initially assigned to the wrong queue and has now been moved to the appropriate SigmaStudio for SHARC eZone support thread.

    To help us better understand and reproduce the issue, could you please confirm the following:

    1. Are the steps you described the exact steps required to reproduce the issue?
    2. What type of input signal are you using during the test? For example, is it a music signal or a sine wave tone?
    3. Have you tried connecting a Level Detector both:
      • At the input of the Compressor, and
      • At the output of the Compressor?

    Monitoring the level at both points will help us understand what is occurring at the compressor input and output when the gain is adjusted, and may provide valuable insight into the root cause of the issue.

    In parallel, we will follow the steps you provided and attempt to reproduce the behavior on our side.

    We appreciate your cooperation and look forward to your response.

  • Hi,
    Reproduction Steps: Yes, the steps I provided earlier are complete and accurate, and they reliably reproduce the issue.

    Test Signal Type: During the test, I used a 1 kHz sine wave tone.

    Regarding Level Detection: I can confirm that the external input signal itself is sufficiently stable. Therefore, I suspect that the issue may be related to the compressor's internal gain calculation logic, rather than being caused by instability in the input signal.

  • Hi,

    Thanks for your valuable input.

    As you mentioned, I was able to reproduce the issue, and the behavior does not match the stable behavior observed in Classic SigmaStudio. The issue has been escalated to the concerned development team for investigation. We are hopeful that a fix can be included in a future SigmaStudio+ release. We will keep you informed of any updates.

    Thanks.

  • Thank you for your support. I look forward to your further updates.

  • The internal team has confirmed that the issue fix is planned for the upcoming v3.5.0 release, which is currently targeted for the end of October.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.