We currently have a custom Pooled Delay block (29 secs) for each channel (12) in our project. It's based on the Pooled Delay sample code, but we have an issue where, if all channels hold a small delay (500ms), then, after some time has passed, the DSP crashes. We think it may be an issue with the custom delay's ASM code but aren't sure. Is there an easier method to doing this? We have gone through the custom delay block's code, but there is little documentation left from the original programmer that there is a possibility that it would be easier to start from fresh than to fix the current code.
We are using the ADSP-21489 with a 64MB/512Mb SDRAM along with SigmaStudio for SHARC 2.2.0 and Crosscore 2.3.0.