Post Go back to editing

Problem with sine wave oscillator in sigma studio+

Thread Summary

The user reported an issue with the sine wave generator in SigmaStudio Plus (v3.3.0) on the SC573 dev board, where the output level gradually increases or decreases at certain frequencies (999Hz and 600Hz) due to floating-point rounding errors. The problem does not occur at 800Hz, 1KHz, or 1.2KHz. The Analog Devices support engineer confirmed the issue and will bring it to the attention of internal teams for resolution. The user created a workaround using the Algorithm Designer, which functions correctly.
AI Generated Content
Category: Software
Product Number: sigma studio+
Software Version: 3.3.0

I am having a problem with the sine wave generator in SS+

for example

If i set the frequency to 999Hz the output level starts increasing very gradually. about 0.001dB per 30 seconds

If i set the frequency to 600Hz the output level starts decreasing very gradually. about 0.001dB per 30 seconds

If i set the frequency to 800Hz, 1KHz or 1.2KHz the output level doesn't move

if i set the phase to something else then back to the intended value i want then the output level returns to the level set in the object settings.

I am using the SC573 dev board and  tried it with Volume_Mute_Block_SC573 example project and also the example project available from the Help menu

- Example for ADSPSC5xx Dual SHCore Demo uC Application 

and converted it for the SC573

I am using the example CCES (v3.0.3.0) project located in SS+ (v3.3.0) C:\Analog Devices\SigmaStudioPlus-Rel3.3.0\Target\Examples\Demo\ADSP-SC57x

To get around the problem i'm having i created my own Sine wave generator using the algorithm designer and it works fine.

 

could you please check if you get the same issue please.

Many thanks

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.