Hi,
I am testing a simple non slewed mute control designed in the algorithm designer
I have the following
EZKIT-573
CCES v3.03
Sigma Studio+ 3.3.0 build 9462 revision 26922
Sigma Studio+ 2.4.0 build 9288 revision 31366
on the CCES i'm running the demo program (no modifications) available in
C:\Analog Devices\SigmaStudioPlus-Rel2.4.0\Target\Examples\Demo\ADSP-SC57x
on SigmaStudio+ i'm using the Volume_Mute_Block_SC573 example project.
I downloaded the example code 'DLB Method Example: Mute (No Slew) Module' from the wiki
wiki.analog.com/.../designermodule
In each version of Sigma Studio+ the MuteNoSlew.dll file worked as expected
I made 2 folders one for each Sigma Studio project and its associated algorithm project.
containing the files needed for each sigma studio version (except the header file)
a folder from extracted downloaded example - 'DLB Method Example: Mute (No Slew) Module' called 'mutenoslew'
SigmaStudio project called 'Volume_Mute_Block_SC573'
In sigma studio project i only added an Algorithm design object in line with an audio channel and opened their algorithm project 'MuteNoSlew.adprj'
The only changes i made to the algoritm project was to use source code and a header file.
for each algorithm project i used the source code in ..\mutenoslew\MuteNoSlew\Src\Srcadi_MuteNoSlew.c
and the header file 'adi_ss_extmod.h' located in C:\Analog Devices\SigmaStudioPlus-Rel2.4.0\Target\Include\ for the Sigma Studio 2.4.0
and 'adi_ss_extmod.h' C:\Analog Devices\SigmaStudioPlus-Rel3.3.0\Target\Include for Sigma Studio 3.3.0
when i used Sigma Studio+ 2.4.0 it worked fine, i could goto 'Manage Runtime Variables' and change the Value of parameter which i could see being written
by looking at the Capture Window. The mute control operated as expected.
When i used exactly the same project in Sigma Studio+ 3.3.0 when i changed the Value, no data was written as observed in the Capture window and nothing happened to the mute operation.
Am i doing something wrong with 3.3.0 as the designer is different or is there a bug in 3.3.0 ?algorithm_tests.zip
attached are the 2 projects i created. You may have to change file locations in the Source and Libraries tab of the algorithm designer as they will show my file locations, not yours
Thanks for any help