Post Go back to editing

When the ADSP-21565 runs at a 96kHz sampling rate, what value should BLOCK_SIZE be set to?

Thread Summary

The user is experiencing noise in the output when using a 21565 DSP with SigmaStudio at 96kHz sampling rate, particularly for sine waves at 800Hz and 1200Hz. The issue persists whether the sine wave is generated by the ADC or within SigmaStudio. The final answer suggests that the block size in SigmaStudio should match the target application's block size, and that noise at high input levels can be mitigated by modifying the utility function. The user confirmed that the issue occurs at both 48kHz and 96kHz, and that sine waves at multiples of 500Hz work fine.
AI Generated Content
Category: Software
Product Number: ADSP-21565
Software Version: cces3.03,sigmastudio4.7

/*****************************************************************************
 * Audio_Loopback_TDM.c
 *****************************************************************************/
#include <stdio.h>
#include <stdlib.h>
#include <sys/platform.h>
#include <sys/adi_core.h>
#include "adi_initialize.h"
#include <services/int/adi_int.h>
#include <drivers/sport/adi_sport.h>
#include <services/pcg/adi_pcg.h>
#include <services/spu/adi_spu.h>
#include <drivers/twi/adi_twi_2156x.h>
#include <services/gpio/adi_gpio.h>
#include "ADAU_1962Common.h"
#include "ADAU_1979Common.h"
#include <cdef21569.h>
#include "math.h"
#include <sru21569.h>
#include "LibIntegrationExample_Core1.h"
#include "adi_ss_smap.h"
#include "PowerServiceConfiguration.h"
#include "adi_ss_ssn_export_T_IC_1.h"
//#include "adi_ss_ssn_export_21565_2_DiffDXESchematic_0.h"
/******* SigmaStudio Integration ***************/

/*Defining Backchannel info structure. Will be populated by the framework */
typedef struct ADI_SS_BACKCH_INFO
{
    float32_t    nPeakMIPS[ADI_SS_FW_MAX_PROC_BLOCKS]; /*!< Peak MIPS for all process blocks */
    float32_t    nAvgMIPS[ADI_SS_FW_MAX_PROC_BLOCKS];  /*!< Average MIPS for all process blocks */
    uint32_t     nVersionInfo;                  	   /*!< Target library API version */
    uint32_t     nSSnDownloadStatus;            	   /*!< Current download status of SSns within all process blocks*/
}ADI_SS_BACKCH_INFO;

#include "adi_ss_connection.h"
#include "adi_ss_communication.h"
#include "adi_ss_ssn.h"

/* Memory for SigmaStudio for Griffin libraries */
/* Connection and Communication Instance Mem */
#pragma align(4)
#pragma section("ss_app_data0_fast")
uint8_t adi_ss_commn_mem[ADI_SS_COMM_MEMSIZE];
#pragma align(4)
#pragma section("ss_app_data0_fast")
uint8_t adi_ss_connection_mem[ADI_SS_CONNECTION_MEMSIZE];

bool bSportCallback;
volatile uint32_t nSMAPReceived=0;

/* SMAP */
ADI_SS_MEM_SMAP oSMAPSharc0;
ADI_SS_MEM_MAP oSSnMemMap;

/* SSn Config structure */
ADI_SS_CONFIG  *pSSnConfig,oSSnConfig;

/* SSnProperties structure */
ADI_SS_SSNPROPERTIES *pSSnProperties,oSSnProperties;

/* Defining SSn Handle */
ADI_SS_SSN_HANDLE hSSnHandle;

/* Backchannel info */
ADI_SS_BACKCH_INFO 	oBkChannelInfoSharc0;

/* I/O buffer and pointers for SSn instance */
float32_t aSSInOutBuff[BLOCK_SIZE*NUM_CHANNELS];


float32_t *pSSInBuff[NUM_CHANNELS];
float32_t *pSSOutBuff[NUM_CHANNELS];

void adi_ss_comm_callback_cmd4(uint32_t  *pCommPayloadBuff,
                               int32_t   nPayloadCount,
                               ADI_SS_SSN_HANDLE hSSn);

void adi_SMAP_Application_Callback(ADI_SS_PROC_ID eCoreID);

/* Convert the audio samples generated by ADC into float format */
void    CopyFix2Float( volatile        uint32_t  *pInBuffer,
                                        uint32_t nInStride,
                       volatile        float    *pOutBuffer,
                                        uint32_t nOutStride,
                                        uint32_t nBlockSize,
                                        uint32_t nShiftFlag);

/* Convert the audio samples from float to fixed point (which can be consumed by DAC) */
uint32_t CopyFloat2Fix(volatile   float *pInBuffer,
                                        uint32_t nInStride,
                               volatile uint32_t *pOutBuffer,
                                        uint32_t nOutStride,
                                        uint32_t nBlockSize,
                                        uint32_t nShiftFlag);

/******* SigmaStudio Integration END  ***************/


/* SPORT buffers */
int32_t int_SP0ABuffer1[BLOCK_SIZE*(NUM_CHANNELS/2)];
int32_t int_SP0ABuffer2[BLOCK_SIZE*(NUM_CHANNELS/2)];
int32_t int_SP0ABuffer3[BLOCK_SIZE*(NUM_CHANNELS/2)];
int32_t int_SP0ABuffer4[BLOCK_SIZE*(NUM_CHANNELS/2)];

int32_t int_SP1ABuffer1[BLOCK_SIZE*(NUM_CHANNELS/2)];
int32_t int_SP1ABuffer2[BLOCK_SIZE*(NUM_CHANNELS/2)];

int32_t int_SP4ABuffer1[BLOCK_SIZE*(NUM_CHANNELS/4)];
int32_t int_SP4ABuffer2[BLOCK_SIZE*(NUM_CHANNELS/4)];
int32_t int_SP4ABuffer3[BLOCK_SIZE*(NUM_CHANNELS/2)];
int32_t int_SP4ABuffer4[BLOCK_SIZE*(NUM_CHANNELS/2)];

int32_t int_SP5ABuffer1[BLOCK_SIZE * (NUM_CHANNELS/2)];
int32_t int_SP5ABuffer2[BLOCK_SIZE * (NUM_CHANNELS/2)];
int32_t int_SP5ABuffer3[BLOCK_SIZE * (NUM_CHANNELS/2)];
int32_t int_SP5ABuffer4[BLOCK_SIZE * (NUM_CHANNELS/2)];

int32_t int_SP6ABuffer1[BLOCK_SIZE * (NUM_CHANNELS/2)];
int32_t int_SP6ABuffer2[BLOCK_SIZE * (NUM_CHANNELS/2)];
int32_t int_SP6ABuffer3[BLOCK_SIZE * (NUM_CHANNELS/2)];
int32_t int_SP6ABuffer4[BLOCK_SIZE * (NUM_CHANNELS/2)];

int32_t int_SP7ABuffer1[BLOCK_SIZE * (NUM_CHANNELS/2)];
int32_t int_SP7ABuffer2[BLOCK_SIZE * (NUM_CHANNELS/2)];
int32_t int_SP7ABuffer3[BLOCK_SIZE * (NUM_CHANNELS/2)];
int32_t int_SP7ABuffer4[BLOCK_SIZE * (NUM_CHANNELS/2)];

struct Config_Table
{
	short Reg_Add;
	char  Value;
};

char Config_read_DAC[28];
char Config_read_ADC[16];
static ADI_PWR_CGU_PARAM_LIST audio_cgu_params = {0};
static ADI_PWR_CDU_PARAM_LIST audio_cdu_params = {0};
/* Dev buffer for configuring ADC-DAC through TWI*/
static uint8_t devBuffer[BUFFER_SIZE];

extern void ConfigSoftSwitches_ADC_DAC(void);

extern void ConfigSoftSwitches_ADAU_Reset(void);

#if 0
struct Config_Table Config_array_DAC[28] = {
		   	    {     ADAU1962_PDN_CTRL_1,		0x00},
		   	    {     ADAU1962_PDN_CTRL_2,	    0xff},
		   	    {     ADAU1962_PDN_CTRL_3,	    0x0f},
		   	    {     ADAU1962_DAC_CTRL0,		0x01},
		   	    {     ADAU1962_DAC_CTRL1,		0x41},
		   	    {     ADAU1962_DAC_CTRL2,		0x00},
		   	    {     ADAU1962_DAC_MUTE1,	    0x0},
		   	    {     ADAU1962_DAC_MUTE2,	    0x00},
		   	    {     ADAU1962_MSTR_VOL,		0x00},
			    {     ADAU1962_DAC1_VOL,	    0x00},
			    {     ADAU1962_DAC2_VOL,		0x00},
				{     ADAU1962_DAC3_VOL,		0x00},
				{     ADAU1962_DAC4_VOL,		0x00},
				{     ADAU1962_DAC5_VOL,		0x00},
				{     ADAU1962_DAC6_VOL,		0x00},
				{     ADAU1962_DAC7_VOL,		0x00},
				{     ADAU1962_DAC8_VOL,	    0x00},
				{     ADAU1962_DAC9_VOL,		0x00},
				{     ADAU1962_DAC10_VOL,		0x00},
				{     ADAU1962_DAC11_VOL,		0x00},
				{     ADAU1962_DAC12_VOL,		0x00},
				{     ADAU1962_PAD_STRGTH,		0x00},
				{     ADAU1962_DAC_PWR1,		0xaa},
				{     ADAU1962_DAC_PWR2,		0xaa},
				{     ADAU1962_DAC_PWR3,		0xaa},
				{     ADAU1962_PDN_CTRL_2,	    0x00},
				{     ADAU1962_PDN_CTRL_3,	    0x00},
				{     ADAU1962_DAC_CTRL0,		0x18}

};
#else
struct Config_Table Config_array_DAC[28] = {
		   	    {     ADAU1962_PDN_CTRL_1,		0xa4 },
		   	    {     ADAU1962_PDN_CTRL_2,	    0xff },  //Power down DAC
		   	    {     ADAU1962_PDN_CTRL_3,	    0x0f }, //Power down DAC
		   	    {     ADAU1962_DAC_CTRL0,		0x19 },
		   	    {     ADAU1962_DAC_CTRL1,		0x63 }, // pulse mode LRCLK, MSB first //orginal value =42
		   	    {     ADAU1962_DAC_CTRL2,		0x04 },  // TDM Configuration
		   	    {     ADAU1962_DAC_MUTE1,	    0x00 },
		   	    {     ADAU1962_DAC_MUTE2,	    0x00 },
		   	    {     ADAU1962_MSTR_VOL,		0x00 },
			    {     ADAU1962_DAC1_VOL,	    0x00 } ,
			    {     ADAU1962_DAC2_VOL,		0x00 },
				{     ADAU1962_DAC3_VOL,		0x00 },
				{     ADAU1962_DAC4_VOL,		0x00 },
				{     ADAU1962_DAC5_VOL,		0x00 },
				{     ADAU1962_DAC6_VOL,		0x00 },
				{     ADAU1962_DAC7_VOL,		0x00 },
				{     ADAU1962_DAC8_VOL,	    0x00 },
				{     ADAU1962_DAC9_VOL,		0x00 },
				{     ADAU1962_DAC10_VOL,		0x00 },
				{     ADAU1962_DAC11_VOL,		0x00 },
				{     ADAU1962_DAC12_VOL,		0x00 },
				{     ADAU1962_PAD_STRGTH,		0x00 },
				{     ADAU1962_DAC_PWR1,		0xaa },
				{     ADAU1962_DAC_PWR2,		0xaa },
				{     ADAU1962_DAC_PWR3,		0xaa },
				{     ADAU1962_PDN_CTRL_2,	    0x00 },
				{     ADAU1962_PDN_CTRL_3,	    0x00 },
		   	    {     ADAU1962_DAC_CTRL0,		0x18 },
};
#endif

#if 0
struct Config_Table Config_array_ADC[16] = {

		 {ADAU1979_REG_BOOST			,	0x00},
		 {ADAU1979_REG_MICBIAS			,	0x00},
		 {ADAU1979_REG_BLOCK_POWER_SAI	,	0x30},
		 /*{ADAU1979_REG_SAI_CTRL0		,	0x1B}, */
		 {ADAU1979_REG_SAI_CTRL0		,	0x1A},/*I2S format*/
		 {ADAU1979_REG_SAI_CTRL1		,	0x08},
		 {ADAU1979_REG_CMAP12			,	0x10},
		 {ADAU1979_REG_CMAP34			,	0x32},
		 {ADAU1979_REG_SAI_OVERTEMP		,	0xf0},
		 {ADAU1979_REG_POST_ADC_GAIN1 	,	0xA0},
		 {ADAU1979_REG_POST_ADC_GAIN2 	,	0xA0},
		 {ADAU1979_REG_POST_ADC_GAIN3 	,	0xA0},
		 {ADAU1979_REG_POST_ADC_GAIN4 	,	0xA0},
		 {ADAU1979_REG_ADC_CLIP			,	0x00},
		 {ADAU1979_REG_DC_HPF_CAL		,	0x00},
		 {ADAU1979_REG_BLOCK_POWER_SAI	,	0x3f},
		 {ADAU1979_REG_MISC_CONTROL		,	0x02}
};
#else
struct Config_Table Config_array_ADC[16] = {

		 {ADAU1979_REG_BOOST			,	0x00},
		 {ADAU1979_REG_MICBIAS			,	0x00},
 		 {ADAU1979_REG_BLOCK_POWER_SAI	,	0xb0},//power down ADC LDO enabel
		 {ADAU1979_REG_SAI_CTRL0		,	0x5a},//TDM 48kHz
		 {ADAU1979_REG_SAI_CTRL1		,	0x08},//LRCLK pulse mode //original value =08
		 {ADAU1979_REG_CMAP12			,	0x10},
		 {ADAU1979_REG_CMAP34			,	0x32},
		 {ADAU1979_REG_SAI_OVERTEMP		,	0xf0},
		 {ADAU1979_REG_POST_ADC_GAIN1 	,	0xA0},
		 {ADAU1979_REG_POST_ADC_GAIN1 	,	0xA0},
		 {ADAU1979_REG_POST_ADC_GAIN3 	,	0xA0},
		 {ADAU1979_REG_POST_ADC_GAIN4 	,	0xA0},
		 {ADAU1979_REG_ADC_CLIP			,	0x00},
		 {ADAU1979_REG_DC_HPF_CAL		,	0x00},// filter off
		 {ADAU1979_REG_BLOCK_POWER_SAI	,	0xbf},//power on  ADC LDO enable
		 {ADAU1979_REG_MISC_CONTROL		,	0x02},//mute all channels
};
#endif

/* Destination PDMA lists */
ADI_PDMA_DESC_LIST iDESC_LIST_1_SP1A;
ADI_PDMA_DESC_LIST iDESC_LIST_2_SP1A ;
ADI_PDMA_DESC_LIST iDESC_LIST_1_SP0A;
ADI_PDMA_DESC_LIST iDESC_LIST_2_SP0A ;
ADI_PDMA_DESC_LIST iDESC_LIST_1_SP6A;
ADI_PDMA_DESC_LIST iDESC_LIST_2_SP6A ;
ADI_PDMA_DESC_LIST iDESC_LIST_1_SP7A;
ADI_PDMA_DESC_LIST iDESC_LIST_2_SP7A ;

/* Source PDMA lists */
ADI_PDMA_DESC_LIST iSRC_LIST_1_SP0B ;
ADI_PDMA_DESC_LIST iSRC_LIST_2_SP0B ;
ADI_PDMA_DESC_LIST iSRC_LIST_1_SP4B ;
ADI_PDMA_DESC_LIST iSRC_LIST_2_SP4B ;
ADI_PDMA_DESC_LIST iSRC_LIST_1_SP5B ;
ADI_PDMA_DESC_LIST iSRC_LIST_2_SP5B ;
ADI_PDMA_DESC_LIST iSRC_LIST_1_SP6B ;
ADI_PDMA_DESC_LIST iSRC_LIST_2_SP6B ;
ADI_PDMA_DESC_LIST iSRC_LIST_1_SP7B ;
ADI_PDMA_DESC_LIST iSRC_LIST_2_SP7B ;

/* Prepares descriptors for SPORT DMA */
static void PrepareDescriptors (void);

/* Count to track the number of callBacks for SPORT transfer */
volatile uint8_t CallbackCount = 0;
volatile uint32_t TestCallbackCount = 0;
volatile uint32_t nDataAvail=0;


/* Memory required for SPORT */
static uint8_t SPORTMemory0B[ADI_SPORT_MEMORY_SIZE];
static uint8_t SPORTMemory0A[ADI_SPORT_MEMORY_SIZE];
static uint8_t SPORTMemory4B[ADI_SPORT_MEMORY_SIZE];
static uint8_t SPORTMemory1A[ADI_SPORT_MEMORY_SIZE];
static uint8_t SPORTMemory5B[ADI_SPORT_MEMORY_SIZE];
static uint8_t SPORTMemory6A[ADI_SPORT_MEMORY_SIZE];
static uint8_t SPORTMemory6B[ADI_SPORT_MEMORY_SIZE];
static uint8_t SPORTMemory7A[ADI_SPORT_MEMORY_SIZE];
static uint8_t SPORTMemory7B[ADI_SPORT_MEMORY_SIZE];
/* SPORT Handle */

static ADI_SPORT_HANDLE hSPORTDev0BRx;
static ADI_SPORT_HANDLE hSPORTDev0ATx;//TX
static ADI_SPORT_HANDLE hSPORTDev4BRx;//RX
static ADI_SPORT_HANDLE hSPORTDev1ATx;//TX
static ADI_SPORT_HANDLE hSPORTDev5BRx;//RX
static ADI_SPORT_HANDLE hSPORTDev6ATx;//TX
static ADI_SPORT_HANDLE hSPORTDev6BRx;//RX
static ADI_SPORT_HANDLE hSPORTDev7ATx;//TX
static ADI_SPORT_HANDLE hSPORTDev7BRx;//RX
/* Memory required for TWI */
uint8_t TwideviceMemory[ADI_TWI_MEMORY_SIZE];

/* TWI driver handle */
static ADI_TWI_HANDLE hTwiDevice;

/* SPU handle */
static ADI_SPU_HANDLE      ghSpu;

/* Memory required for the SPU operation */
uint8_t             SpuMemory[ADI_SPU_MEMORY_SIZE];

int32_t delay;

static int32_t ADAU_1962_Pllinit(void);
static int32_t ADAU_1979_Pllinit(void);
void Switch_Configurator(void);
static int32_t ADAU_1962_init(void);
static int32_t ADAU_1979_init(void);
void SRU_Init(void);
static int32_t Sport_Init(void);
static int32_t Sport_Stop(void);
static int32_t SPU_init(void);
static void PrepareDescriptors (void);
static int32_t Init_TWI(void);
static int32_t Stop_TWI(void);
void PCG_init(void);



static void SPORTCallback(void        *pAppHandle,
						  uint32_t     nEvent,
						  void        *pArg
						 )
{
	int32_t i;
	int32_t j;

	ADI_SPORT_RESULT eResult;
    /* CASEOF (event type) */
    switch (nEvent)
    {
        /* CASE (buffer processed) */
        case ADI_SPORT_EVENT_RX_BUFFER_PROCESSED:
        		CallbackCount += 1;
        		nDataAvail += 1;
        		break;
        default:
        	 break;
    }
    /* return */
}
uint32_t adi_pwr_audio_config(void)
{
	ADI_PWR_CGU_PARAM_LIST pADI_CGU_Param_List;
	    ADI_PWR_CDU_PARAM_LIST pADI_CDU_Param_List;

	    audio_cgu_params.cgu0_settings.clocksettings.ctl_MSEL = 80; // PLL=CLKIN*MSEL
	    audio_cgu_params.cgu0_settings.clocksettings.ctl_DF = 0; // DF=0
	    audio_cgu_params.cgu0_settings.clocksettings.div_CSEL = 2; // CCLK = PLL/CCLK =
	    audio_cgu_params.cgu0_settings.clocksettings.div_SYSSEL = 4; // SYSCLK = CCLK/SYSSEL =
	    audio_cgu_params.cgu0_settings.clocksettings.div_S0SEL = 4; // SCLK0 = SYSCLK/S0SEL =
	    audio_cgu_params.cgu0_settings.clocksettings.div_DSEL = 6; // DCLK = PLLCLK/6 ≈
	    audio_cgu_params.cgu0_settings.clocksettings.div_OSEL = 16; // OCLK = PLLCLK/16 =
	    //audio_cgu_params.cgu0_settings.clkin = 25000000; // 25MHz输入
	    audio_cgu_params.cgu0_settings.clkin = 24576000;
	    /* 2. 配置CDU参数 - 使用SCLK0作为CLKO0输出 */
	    audio_cdu_params.cdu_settings[0].cfg_SEL = 0; // 对应SCLK0_0
	    audio_cdu_params.cdu_settings[0].cfg_EN = true;

	    /* 3. 初始化时钟系统 - 仅使用CGU0 */
	    audio_cgu_params.cgu1_settings.clocksettings.ctl_MSEL = 0; // 禁用CGU1

	    /* 调用原文件中的时钟初始化函数 */
	    if(adi_pwr_ClockInit(&audio_cgu_params, &audio_cdu_params) != ADI_PWR_SUCCESS)
	    {
	        return 1u; // 初始化失败
	    }

	    return 0u; // 初始化成功
}

/* 主配置函数 */
uint32_t adi_pwr_cfg0_init(void)
{
	 /* 调用自定义音频配置 */
	    if(adi_pwr_audio_config() != 0u)
	    {
	        return 1u;
	    }

	    return 0u;
}

void PCG_init(void)
{
	 ADI_PCG_CLK_INFO gClkInfoA = {
			 ADI_PCG_CLK_CLKIN0, // Clock Source
	        1, // Clock Divisor
	        false // External Trigger
	    };

	    ADI_PCG_FS_INFO gFsInfoA = {
	    		ADI_PCG_CLK_CLKIN0, // Clock Source
	        256,
	        128,
	        0, // Phase
	        false, // External Trigger
	        ADI_PCG_FSBYPASS_MODE_NORMAL // Bypass Mode
	    };

	    ADI_PCG_CLK_INFO gClkInfoC = {
	    		ADI_PCG_CLK_EXT, // Clock Source
	   	        1, // Clock Divisor
	   	        false // External Trigger
	   	    };

	   	    ADI_PCG_FS_INFO gFsInfoC = {
	   	    		ADI_PCG_CLK_EXT, // Clock Source
	   	        256, // Frame Sync Divisor (256 for 48kHz)
	   	        128, // Pulse Width (16 slots * 32 bits)
	   	        0, // Phase
	   	        false, // External Trigger
	   	        ADI_PCG_FSBYPASS_MODE_NORMAL // Bypass Mode
	   	    };
	   	 ADI_PCG_CLK_INFO gClkInfoB = {
	   			 	 	 ADI_PCG_CLK_EXT, // Clock Source
	   	 	   	       1, // Clock Divisor
	   	 	   	        false // External Trigger
	   	 	   	    };

	   	 	   	    ADI_PCG_FS_INFO gFsInfoB = {
	   	 	   	    	ADI_PCG_CLK_EXT, // Clock Source
	   	 	   	        256, // Frame Sync Divisor (256 for 48kHz)
	   	 	   	        128, // Pulse Width (16 slots * 32 bits)
	   	 	   	        0, // Phase
	   	 	   	        false, // External Trigger
	   	 	   	        ADI_PCG_FSBYPASS_MODE_NORMAL // Bypass Mode
	   	 	   	    };

	    adi_pcg_Init(ADI_PCG_DEV_A, &gClkInfoA, &gFsInfoA);
	    adi_pcg_Init(ADI_PCG_DEV_B, &gClkInfoB, &gFsInfoB);
	    adi_pcg_Init(ADI_PCG_DEV_C, &gClkInfoC, &gFsInfoC);
}
/*
 * Prepares descriptors for Memory DMA copy.
 *
 * Parameters
 *  None
 *
 * Returns
 *  None
 *
 */

static void PrepareDescriptors (void)
{

	iSRC_LIST_1_SP0B.pStartAddr		=(int32_t *)int_SP0ABuffer3;
	iSRC_LIST_1_SP0B.Config			= ENUM_DMA_CFG_XCNT_INT ;
	iSRC_LIST_1_SP0B.XCount			= BLOCK_SIZE*(NUM_CHANNELS/3);
	iSRC_LIST_1_SP0B.XModify		= 4;
	iSRC_LIST_1_SP0B.YCount			= 0;
	iSRC_LIST_1_SP0B.YModify		= 0;
	iSRC_LIST_1_SP0B.pNxtDscp		= &iSRC_LIST_2_SP0B;

	iSRC_LIST_2_SP0B.pStartAddr		=(int32_t *)int_SP0ABuffer4;
	iSRC_LIST_2_SP0B.Config			= ENUM_DMA_CFG_XCNT_INT;
	iSRC_LIST_2_SP0B.XCount			= BLOCK_SIZE*(NUM_CHANNELS/3);
	iSRC_LIST_2_SP0B.XModify		= 4;
	iSRC_LIST_2_SP0B.YCount			= 0;
	iSRC_LIST_2_SP0B.YModify		= 0;
	iSRC_LIST_2_SP0B.pNxtDscp		= &iSRC_LIST_1_SP0B;

	iDESC_LIST_1_SP0A.pStartAddr	= (int32_t *)int_SP4ABuffer3;
	iDESC_LIST_1_SP0A.Config		= ENUM_DMA_CFG_XCNT_INT ;
	iDESC_LIST_1_SP0A.XCount		= BLOCK_SIZE*(NUM_CHANNELS/2);
	iDESC_LIST_1_SP0A.XModify		= 4;
	iDESC_LIST_1_SP0A.YCount		= 0;
	iDESC_LIST_1_SP0A.YModify		= 0;
	iDESC_LIST_1_SP0A.pNxtDscp		= &iDESC_LIST_2_SP0A;

	iDESC_LIST_2_SP0A.pStartAddr	= (int32_t *)int_SP4ABuffer4;
	iDESC_LIST_2_SP0A.Config		= ENUM_DMA_CFG_XCNT_INT ;
	iDESC_LIST_2_SP0A.XCount		= BLOCK_SIZE*(NUM_CHANNELS/2);
	iDESC_LIST_2_SP0A.XModify		= 4;
	iDESC_LIST_2_SP0A.YCount		= 0;
	iDESC_LIST_2_SP0A.YModify		= 0;
	iDESC_LIST_2_SP0A.pNxtDscp		= &iDESC_LIST_1_SP0A;

	iSRC_LIST_1_SP4B.pStartAddr		=(int32_t *)int_SP4ABuffer3;
	iSRC_LIST_1_SP4B.Config			= ENUM_DMA_CFG_XCNT_INT ;
	iSRC_LIST_1_SP4B.XCount			= BLOCK_SIZE*(NUM_CHANNELS/2);
	iSRC_LIST_1_SP4B.XModify		= 4;
	iSRC_LIST_1_SP4B.YCount			= 0;
	iSRC_LIST_1_SP4B.YModify		= 0;
	iSRC_LIST_1_SP4B.pNxtDscp		= &iSRC_LIST_2_SP4B;

	iSRC_LIST_2_SP4B.pStartAddr		=(int32_t *)int_SP4ABuffer4;
	iSRC_LIST_2_SP4B.Config			= ENUM_DMA_CFG_XCNT_INT;
	iSRC_LIST_2_SP4B.XCount			= BLOCK_SIZE*(NUM_CHANNELS/2);
	iSRC_LIST_2_SP4B.XModify		= 4;
	iSRC_LIST_2_SP4B.YCount			= 0;
	iSRC_LIST_2_SP4B.YModify		= 0;
	iSRC_LIST_2_SP4B.pNxtDscp		= &iSRC_LIST_1_SP4B;

	iDESC_LIST_1_SP1A.pStartAddr	= (int32_t *)int_SP5ABuffer3;
	iDESC_LIST_1_SP1A.Config		= ENUM_DMA_CFG_XCNT_INT ;
	iDESC_LIST_1_SP1A.XCount		= BLOCK_SIZE*(NUM_CHANNELS/2);
	iDESC_LIST_1_SP1A.XModify		= 4;
	iDESC_LIST_1_SP1A.YCount		= 0;
	iDESC_LIST_1_SP1A.YModify		= 0;
	iDESC_LIST_1_SP1A.pNxtDscp		= &iDESC_LIST_2_SP1A;

	iDESC_LIST_2_SP1A.pStartAddr	= (int32_t *)int_SP5ABuffer4;
	iDESC_LIST_2_SP1A.Config		= ENUM_DMA_CFG_XCNT_INT ;
	iDESC_LIST_2_SP1A.XCount		= BLOCK_SIZE*(NUM_CHANNELS/2);
	iDESC_LIST_2_SP1A.XModify		= 4;
	iDESC_LIST_2_SP1A.YCount		= 0;
	iDESC_LIST_2_SP1A.YModify		= 0;
	iDESC_LIST_2_SP1A.pNxtDscp		= &iDESC_LIST_1_SP1A;

	iSRC_LIST_1_SP5B.pStartAddr		=(int32_t *)int_SP5ABuffer3;
	iSRC_LIST_1_SP5B.Config			= ENUM_DMA_CFG_XCNT_INT ;
	iSRC_LIST_1_SP5B.XCount			= BLOCK_SIZE*(NUM_CHANNELS/2);
	iSRC_LIST_1_SP5B.XModify		= 4;
	iSRC_LIST_1_SP5B.YCount			= 0;
	iSRC_LIST_1_SP5B.YModify		= 0;
	iSRC_LIST_1_SP5B.pNxtDscp		= &iSRC_LIST_2_SP5B;

	iSRC_LIST_2_SP5B.pStartAddr		=(int32_t *)int_SP5ABuffer4;
	iSRC_LIST_2_SP5B.Config			= ENUM_DMA_CFG_XCNT_INT;
	iSRC_LIST_2_SP5B.XCount			= BLOCK_SIZE*(NUM_CHANNELS/2);
	iSRC_LIST_2_SP5B.XModify		= 4;
	iSRC_LIST_2_SP5B.YCount			= 0;
	iSRC_LIST_2_SP5B.YModify		= 0;
	iSRC_LIST_2_SP5B.pNxtDscp		= &iSRC_LIST_1_SP5B;

	iDESC_LIST_1_SP6A.pStartAddr	= (int32_t *)int_SP6ABuffer1;
	iDESC_LIST_1_SP6A.Config		= ENUM_DMA_CFG_XCNT_INT ;
	iDESC_LIST_1_SP6A.XCount		= BLOCK_SIZE*(NUM_CHANNELS/2);
	iDESC_LIST_1_SP6A.XModify		= 4;
	iDESC_LIST_1_SP6A.YCount		= 0;
	iDESC_LIST_1_SP6A.YModify		= 0;
	iDESC_LIST_1_SP6A.pNxtDscp		= &iDESC_LIST_2_SP6A;

	iDESC_LIST_2_SP6A.pStartAddr	= (int32_t *)int_SP6ABuffer2;
	iDESC_LIST_2_SP6A.Config		= ENUM_DMA_CFG_XCNT_INT ;
	iDESC_LIST_2_SP6A.XCount		= BLOCK_SIZE*(NUM_CHANNELS/2);
	iDESC_LIST_2_SP6A.XModify		= 4;
	iDESC_LIST_2_SP6A.YCount		= 0;
	iDESC_LIST_2_SP6A.YModify		= 0;
	iDESC_LIST_2_SP6A.pNxtDscp		= &iDESC_LIST_1_SP6A;

	iSRC_LIST_1_SP6B.pStartAddr		=(int32_t *)int_SP6ABuffer3;
	iSRC_LIST_1_SP6B.Config			= ENUM_DMA_CFG_XCNT_INT ;
	iSRC_LIST_1_SP6B.XCount			= BLOCK_SIZE*(NUM_CHANNELS/6);
	iSRC_LIST_1_SP6B.XModify		= 4;
	iSRC_LIST_1_SP6B.YCount			= 0;
	iSRC_LIST_1_SP6B.YModify		= 0;
	iSRC_LIST_1_SP6B.pNxtDscp		= &iSRC_LIST_2_SP6B;

	iSRC_LIST_2_SP6B.pStartAddr		=(int32_t *)int_SP6ABuffer4;
	iSRC_LIST_2_SP6B.Config			= ENUM_DMA_CFG_XCNT_INT;
	iSRC_LIST_2_SP6B.XCount			= BLOCK_SIZE*(NUM_CHANNELS/6);
	iSRC_LIST_2_SP6B.XModify		= 4;
	iSRC_LIST_2_SP6B.YCount			= 0;
	iSRC_LIST_2_SP6B.YModify		= 0;
	iSRC_LIST_2_SP6B.pNxtDscp		= &iSRC_LIST_1_SP6B;

	iDESC_LIST_1_SP7A.pStartAddr	= (int32_t *)int_SP7ABuffer1;
	iDESC_LIST_1_SP7A.Config		= ENUM_DMA_CFG_XCNT_INT ;
	iDESC_LIST_1_SP7A.XCount		= BLOCK_SIZE*(NUM_CHANNELS/2);
	iDESC_LIST_1_SP7A.XModify		= 4;
	iDESC_LIST_1_SP7A.YCount		= 0;
	iDESC_LIST_1_SP7A.YModify		= 0;
	iDESC_LIST_1_SP7A.pNxtDscp		= &iDESC_LIST_2_SP7A;

	iDESC_LIST_2_SP7A.pStartAddr	= (int32_t *)int_SP7ABuffer2;
	iDESC_LIST_2_SP7A.Config		= ENUM_DMA_CFG_XCNT_INT ;
	iDESC_LIST_2_SP7A.XCount		= BLOCK_SIZE*(NUM_CHANNELS/2);
	iDESC_LIST_2_SP7A.XModify		= 4;
	iDESC_LIST_2_SP7A.YCount		= 0;
	iDESC_LIST_2_SP7A.YModify		= 0;
	iDESC_LIST_2_SP7A.pNxtDscp		= &iDESC_LIST_1_SP7A;

	iSRC_LIST_1_SP7B.pStartAddr		=(int32_t *)int_SP7ABuffer3;
	iSRC_LIST_1_SP7B.Config			= ENUM_DMA_CFG_XCNT_INT ;
	iSRC_LIST_1_SP7B.XCount			= BLOCK_SIZE*(NUM_CHANNELS/6);
	iSRC_LIST_1_SP7B.XModify		= 4;
	iSRC_LIST_1_SP7B.YCount			= 0;
	iSRC_LIST_1_SP7B.YModify		= 0;
	iSRC_LIST_1_SP7B.pNxtDscp		= &iSRC_LIST_2_SP7B;

	iSRC_LIST_2_SP7B.pStartAddr		=(int32_t *)int_SP7ABuffer4;
	iSRC_LIST_2_SP7B.Config			= ENUM_DMA_CFG_XCNT_INT;
	iSRC_LIST_2_SP7B.XCount			= BLOCK_SIZE*(NUM_CHANNELS/6);
	iSRC_LIST_2_SP7B.XModify		= 4;
	iSRC_LIST_2_SP7B.YCount			= 0;
	iSRC_LIST_2_SP7B.YModify		= 0;
	iSRC_LIST_2_SP7B.pNxtDscp		= &iSRC_LIST_1_SP7B;
}

static int32_t Sport_Init()
{

	    /* SPORT return code */
	    ADI_SPORT_RESULT eResult;

	    /* Open SPORT Device 0A (TX) */
	    eResult = adi_sport_Open(SPORT_DEVICE_0A, ADI_HALF_SPORT_A, ADI_SPORT_DIR_TX,
	                             ADI_SPORT_MC_MODE,
	                             SPORTMemory0A, ADI_SPORT_MEMORY_SIZE, &hSPORTDev0ATx);
	    CHECK_RESULT(eResult);



	    /* Open SPORT Device 4B (RX) */
	    eResult = adi_sport_Open(SPORT_DEVICE_4B, ADI_HALF_SPORT_B, ADI_SPORT_DIR_RX,
	                             ADI_SPORT_MC_MODE,
	                             SPORTMemory4B, ADI_SPORT_MEMORY_SIZE, &hSPORTDev4BRx);
	    CHECK_RESULT(eResult);

	    /* Open SPORT Device 1A (TX) */
	    eResult = adi_sport_Open(SPORT_DEVICE_1A, ADI_HALF_SPORT_A, ADI_SPORT_DIR_TX,
	                             ADI_SPORT_MC_MODE,
	                             SPORTMemory1A, ADI_SPORT_MEMORY_SIZE, &hSPORTDev1ATx);
	    CHECK_RESULT(eResult);

	    /* Open SPORT Device 5B (RX) */
	    eResult = adi_sport_Open(SPORT_DEVICE_5B, ADI_HALF_SPORT_B, ADI_SPORT_DIR_RX,
	                             ADI_SPORT_MC_MODE,
	                             SPORTMemory5B, ADI_SPORT_MEMORY_SIZE, &hSPORTDev5BRx);
	    CHECK_RESULT(eResult);

	    /* Configure data, clock, frame sync and MCTL of SPORT Device 0A */
	    eResult = adi_sport_ConfigData(hSPORTDev0ATx, ADI_SPORT_DTYPE_ZERO_FILL, 31, false, false, false);
	    CHECK_RESULT(eResult);

	    eResult = adi_sport_ConfigClock(hSPORTDev0ATx, 32, false, /*false*/ false, false);
	    CHECK_RESULT(eResult);

	    eResult = adi_sport_ConfigFrameSync(hSPORTDev0ATx, 31, false, false, false, /*true*/ true, false, false);
	    CHECK_RESULT(eResult);

	    eResult = adi_sport_ConfigMC(hSPORTDev0ATx, 1u, 7u, 0u, false);
	    CHECK_RESULT(eResult);

	    eResult = adi_sport_SelectChannel(hSPORTDev0ATx, 0u, 7u);
	    CHECK_RESULT(eResult);

	#if 1
		eResult = adi_sport_Open(SPORT_DEVICE_0B,ADI_HALF_SPORT_B,ADI_SPORT_DIR_RX, ADI_SPORT_I2S_MODE, SPORTMemory0B,ADI_SPORT_MEMORY_SIZE,&hSPORTDev0BRx);
		CHECK_RESULT(eResult);
	#endif

	    /* Configure data, clock, frame sync and MCTL of SPORT Device 4B */
	    eResult = adi_sport_ConfigData(hSPORTDev4BRx, ADI_SPORT_DTYPE_ZERO_FILL, 31, false, false, false);
	    CHECK_RESULT(eResult);

	    eResult = adi_sport_ConfigClock(hSPORTDev4BRx, 32, false, /*false*/ false, false);
	    CHECK_RESULT(eResult);

	    eResult = adi_sport_ConfigFrameSync(hSPORTDev4BRx, 31, false, false, false, /*true*/ true, false, false);
	    CHECK_RESULT(eResult);

	    eResult = adi_sport_ConfigMC(hSPORTDev4BRx, 1u, 7u, 0u, false);
	    CHECK_RESULT(eResult);

	    eResult = adi_sport_SelectChannel(hSPORTDev4BRx, 0u, 7u);
	    CHECK_RESULT(eResult);

	    /* Configure data, clock, frame sync and MCTL of SPORT Device 1A */
	    eResult = adi_sport_ConfigData(hSPORTDev1ATx, ADI_SPORT_DTYPE_ZERO_FILL, 31, false, false, false);
	    CHECK_RESULT(eResult);

	    eResult = adi_sport_ConfigClock(hSPORTDev1ATx, 32, false, /*false*/ false, false);
	    CHECK_RESULT(eResult);

	    eResult = adi_sport_ConfigFrameSync(hSPORTDev1ATx, 31, false, false, false, /*true*/ true, false, false);
	    CHECK_RESULT(eResult);

	    eResult = adi_sport_ConfigMC(hSPORTDev1ATx, 1u, 7u, 0u, false);
	    CHECK_RESULT(eResult);

	    eResult = adi_sport_SelectChannel(hSPORTDev1ATx, 0u, 7u);
	    CHECK_RESULT(eResult);

	    /* Configure data, clock, frame sync and MCTL of SPORT Device 5B */
	    eResult = adi_sport_ConfigData(hSPORTDev5BRx, ADI_SPORT_DTYPE_ZERO_FILL, 31, false, false, false);
	    CHECK_RESULT(eResult);

	    eResult = adi_sport_ConfigClock(hSPORTDev5BRx, 32, false, /*false*/ false, false);
	    CHECK_RESULT(eResult);

	    eResult = adi_sport_ConfigFrameSync(hSPORTDev5BRx, 31, false, false, false, /*true*/ true, false, false);
	    CHECK_RESULT(eResult);

	    eResult = adi_sport_ConfigMC(hSPORTDev5BRx, 1u, 7u, 0u, false);
	    CHECK_RESULT(eResult);

	    eResult = adi_sport_SelectChannel(hSPORTDev5BRx, 0u, 7u);
	    CHECK_RESULT(eResult);

	    /* Register SPORT Callback function */
	    eResult = adi_sport_RegisterCallback(hSPORTDev4BRx, SPORTCallback, NULL);
	    CHECK_RESULT(eResult);
	    eResult = adi_sport_RegisterCallback(hSPORTDev5BRx, SPORTCallback, NULL);
	    CHECK_RESULT(eResult);

	    /* Prepare descriptors */
	    PrepareDescriptors();

	    /* Submit the first buffer for RX */
	    eResult = adi_sport_DMATransfer(hSPORTDev4BRx, &iSRC_LIST_1_SP4B, (DMA_NUM_DESC), ADI_PDMA_DESCRIPTOR_LIST,
	                                    ADI_SPORT_CHANNEL_PRIM);
	    CHECK_RESULT(eResult);

	    eResult = adi_sport_DMATransfer(hSPORTDev0BRx, &iSRC_LIST_1_SP0B, (DMA_NUM_DESC), ADI_PDMA_DESCRIPTOR_LIST,
	                                    ADI_SPORT_CHANNEL_PRIM);
	    CHECK_RESULT(eResult);

	    /* Submit the first buffer for TX */
	    eResult = adi_sport_DMATransfer(hSPORTDev0ATx, &iDESC_LIST_1_SP0A, (DMA_NUM_DESC), ADI_PDMA_DESCRIPTOR_LIST,
	                                    ADI_SPORT_CHANNEL_PRIM);
	    CHECK_RESULT(eResult);

	    /* Submit the first buffer for RX */
	    eResult = adi_sport_DMATransfer(hSPORTDev5BRx, &iSRC_LIST_1_SP5B, (DMA_NUM_DESC), ADI_PDMA_DESCRIPTOR_LIST,
	                                    ADI_SPORT_CHANNEL_PRIM);
	    CHECK_RESULT(eResult);

	    /* Submit the first buffer for TX */
	    eResult = adi_sport_DMATransfer(hSPORTDev1ATx, &iDESC_LIST_1_SP1A, (DMA_NUM_DESC), ADI_PDMA_DESCRIPTOR_LIST,
	                                    ADI_SPORT_CHANNEL_PRIM);
	    CHECK_RESULT(eResult);

	    /* Enable SPORT Device 5B */
	    eResult = adi_sport_Enable(hSPORTDev5BRx, true);
	    CHECK_RESULT(eResult);

	    eResult = adi_sport_Enable(hSPORTDev0BRx, true);
	    CHECK_RESULT(eResult);

	    /* Enable SPORT Device 1A */
	    eResult = adi_sport_Enable(hSPORTDev1ATx, true);
	    CHECK_RESULT(eResult);

	    /* Enable SPORT Device 4B */
	    eResult = adi_sport_Enable(hSPORTDev4BRx, true);
	    CHECK_RESULT(eResult);

	    /* Enable SPORT Device 0A */
	    eResult = adi_sport_Enable(hSPORTDev0ATx, true);
	    CHECK_RESULT(eResult);

	    return eResult;
}




static int32_t Sport_Stop(void)
{
	  /* SPORT return code */
	    ADI_SPORT_RESULT eResult;

	    /* Stop DMA transfer of SPORT Device 4B */
	    eResult = adi_sport_StopDMATransfer(hSPORTDev4BRx);
	    CHECK_RESULT(eResult);

	    eResult = adi_sport_StopDMATransfer(hSPORTDev0BRx);
	    CHECK_RESULT(eResult);

	    /* Stop DMA transfer of SPORT Device 0A */
	    eResult = adi_sport_StopDMATransfer(hSPORTDev0ATx);
	    CHECK_RESULT(eResult);

	    /* Stop DMA transfer of SPORT Device 5B */
	    eResult = adi_sport_StopDMATransfer(hSPORTDev5BRx);
	    CHECK_RESULT(eResult);

	    /* Stop DMA transfer of SPORT Device 1A */
	    eResult = adi_sport_StopDMATransfer(hSPORTDev1ATx);
	    CHECK_RESULT(eResult);

	    /* Close SPORT Device 4B */
	    eResult = adi_sport_Close(hSPORTDev4BRx);
	    CHECK_RESULT(eResult);

	    eResult = adi_sport_Close(hSPORTDev0BRx);
	    CHECK_RESULT(eResult);

	    /* Close SPORT Device 0A */
	    eResult = adi_sport_Close(hSPORTDev0ATx);
	    CHECK_RESULT(eResult);

	    /* Close SPORT Device 5B */
	    eResult = adi_sport_Close(hSPORTDev5BRx);
	    CHECK_RESULT(eResult);

	    /* Close SPORT Device 1A */
	    eResult = adi_sport_Close(hSPORTDev1ATx);
	    CHECK_RESULT(eResult);

	    return eResult;
}

/*
 * Prepares Switch configuration.
 *
 * Parameters
 *  None
 *
 * Returns
 *  None
 *
 */
void Switch_Configurator()
{
	int32_t delay11=0xffff;


	/* Software Switch Configuration for Re-Setting ADC-DAC  */
	ConfigSoftSwitches_ADAU_Reset();

	while(delay11--)
	{
		asm("nop;");
	}

	/* Software Switch Configuration for Enabling ADC-DAC */
	ConfigSoftSwitches_ADC_DAC();

	/* wait for Codec to up */
	delay11=0xffff;
	while(delay11--)
	{
		asm("nop;");
	}
}



/*
 * Prepares SRU configuration.
 *
 * Parameters
 *  None
 *
 * Returns
 *  None
 *
 */
void SRU_Init()
{
	*pREG_PADS0_DAI0_IE=0xfffff;
	*pREG_PADS0_DAI1_IE=0xfffff;
	*pREG_PADS0_DAI0_0_DS=0x12492492;
	//*pREG_PADS0_DAI0_0_DS = 0x00240249;

	 SRU(HIGH,DAI0_PBEN01_I);//
	 SRU(HIGH,DAI0_PBEN02_I);//
	 SRU(HIGH,DAI0_PBEN03_I);//
	 SRU(HIGH,DAI0_PBEN04_I);//
	 SRU(LOW,DAI0_PBEN05_I);
	 SRU(HIGH,DAI0_PBEN06_I);//
	 SRU(HIGH,DAI0_PBEN07_I);//
	 SRU(HIGH,DAI0_PBEN08_I);//
	 SRU(HIGH,DAI0_PBEN09_I);//
	 SRU(HIGH,DAI0_PBEN10_I);//
	 SRU(HIGH,DAI0_PBEN19_I);//
	 SRU(HIGH,DAI0_PBEN20_I);//

	 SRU2(LOW,DAI1_PBEN01_I);
	 SRU2(LOW,DAI1_PBEN02_I);
	 SRU2(LOW,DAI1_PBEN03_I);
	 SRU2(HIGH,DAI1_PBEN04_I);//
	 SRU2(LOW,DAI1_PBEN05_I);
	 SRU2(LOW,DAI1_PBEN06_I);
	 SRU2(LOW,DAI1_PBEN07_I);
	 SRU2(LOW,DAI1_PBEN08_I);
	 SRU2(LOW,DAI1_PBEN09_I);
	 SRU2(LOW,DAI1_PBEN10_I);
	 SRU2(LOW,DAI1_PBEN19_I);
	 SRU2(LOW,DAI1_PBEN20_I);

	 //9039
#if 1
 	 SRU2(PCG0_CRS_CLKA_O,DAI1_PB04_I);//BCLK
 	 //SRU2(DAI1_PB05_O,DAI1_PB04_I);
 	 SRU(PCG0_FSA_O,DAI0_PB02_I);//LRCLK
 	 SRU(PCG0_CLKA_O,DAI0_PB01_I);//BCLK
 	 SRU(PCG0_FSA_O,SPT0_AFS_I);//LRCLK
 	 SRU(PCG0_CLKA_O,SPT0_ACLK_I);//BCLK
 	 SRU(PCG0_FSA_O,SPT1_AFS_I);//LRCLK
 	 SRU(PCG0_CLKA_O,SPT1_ACLK_I);//BCLK

 	 SRU(SPT1_AD0_O,DAI0_PB03_I);//DATA1
 	 SRU(SPT0_AD0_O,DAI0_PB07_I);//DATA2
 	 SRU(SPT0_AD0_O,DAI0_PB04_I);//DATA1
 	 SRU(SPT1_AD0_O,DAI0_PB08_I);

 	 SRU2(DAI1_PB06_O,SPT4_BFS_I);//LRCLK
 	 SRU2(DAI1_PB05_O,SPT4_BCLK_I);//BCLK
 	 SRU2(DAI1_PB06_O,SPT5_BFS_I);//LRCLK
 	 SRU2(DAI1_PB05_O,SPT5_BCLK_I);//BCLK
 	 SRU2(DAI1_PB09_O,SPT4_BD0_I);//DATA1
 	 SRU2(DAI1_PB10_O,SPT5_BD0_I);//DATA2
#endif


#if 0
	 SRU2(DAI1_PB05_O,PCG0_EXTCLKC_I);
	 	 SRU(PCG0_CRS_FSC_O,DAI0_PB02_I);//LRCLK
	 	 SRU(PCG0_CRS_CLKC_O,DAI0_PB01_I);//BCLK
	 	 SRU(DAI0_PB02_O,SPT0_AFS_I);//LRCLK
	 	 SRU(DAI0_PB01_O,SPT0_ACLK_I);//BCLK
	 	 SRU(DAI0_PB02_O,SPT1_AFS_I);//LRCLK
	 	 SRU(DAI0_PB01_O,SPT1_ACLK_I);//BCLK

	 	 SRU(SPT1_AD0_O,DAI0_PB03_I);//DATA1
	 	 SRU(SPT0_AD0_O,DAI0_PB07_I);//DATA2
	 	 SRU(SPT0_AD0_O,DAI0_PB04_I);//DATA1
	 	 SRU(SPT1_AD0_O,DAI0_PB08_I);

	 	 //SRU(DAI0_PB07_O,DAI0_PB07_I);//DATA1
	 	// SRU(DAI0_PB08_O,DAI0_PB08_I);//DATA2
	 //OTG
	 	// SRU2(DAI1_PB07_O,SPT4_AFS_I);//LRCLK
	 	 SRU2(DAI1_PB05_O,DAI1_PB04_I);//BCLK
	 	// SRU2(DAI1_PB08_O,SPT4_AD0_I);//DATA1
	 //BT
	 	// SRU2(DAI1_PB01_O,SPT4_AD0_I);//BCLK
	 	// SRU2(DAI1_PB02_O,SPT4_AD0_I);//LRCLK
	 	// SRU2(DAI1_PB03_O,SPT4_AD0_I);//DATA
	 //DSP1 TO DSP2
	 	 SRU2(DAI1_PB06_O,SPT4_BFS_I);//LRCLK
	 	 SRU2(DAI1_PB05_O,SPT4_BCLK_I);//BCLK
	 	 SRU2(DAI1_PB06_O,SPT5_BFS_I);//LRCLK
	 	 SRU2(DAI1_PB05_O,SPT5_BCLK_I);//BCLK
	 	 SRU2(DAI1_PB09_O,SPT4_BD0_I);//DATA1
	 	 SRU2(DAI1_PB10_O,SPT5_BD0_I);//DATA2
	 	 //SRU2(DAI1_PB19_O,DAI1_PB02_I);//DATA3
	 	//SRU2(DAI1_PB20_O,DAI1_PB01_I);//DATA4
	 //DSP2 TO DSP1
	 	 //SRU(DAI0_PB10_O,DAI0_PB09_I);//LRCLK
	 	 //SRU(DAI0_PB19_O,DAI0_PB10_I);//BCLK
#endif
}
/*
 * Prepares SPU configuration.
 *
 * Parameters
 *  None
 *
 * Returns
 *  None
 *
 */
int32_t SPU_init(void)
{
    if(adi_spu_Init(0, SpuMemory, NULL, NULL, &ghSpu) != ADI_SPU_SUCCESS)
    {
    	REPORT_ERROR("Failed to initialize SPU service\n");
		return FAILED;
    }

    /* Make SPORT 0A to generate secure transactions */
    if(adi_spu_EnableMasterSecure(ghSpu, SPORT_0A_SPU, true) != ADI_SPU_SUCCESS)
    {
    	REPORT_ERROR("Failed to enable Master secure for SPORT0A\n");
		return FAILED;
    }

    /* Make SPORT 0B to generate secure transactions */
    if(adi_spu_EnableMasterSecure(ghSpu, SPORT_4B_SPU, true) != ADI_SPU_SUCCESS)
    {
    	REPORT_ERROR("Failed to enable Master secure for SPORT0B\n");
		return FAILED;
    }
    if(adi_spu_EnableMasterSecure(ghSpu, SPORT_0B_SPU, true) != ADI_SPU_SUCCESS)
    {
    	REPORT_ERROR("Failed to enable Master secure for SPORT0B\n");
		return FAILED;
    }
    if(adi_spu_EnableMasterSecure(ghSpu, SPORT_1A_SPU, true) != ADI_SPU_SUCCESS)
       {
       	REPORT_ERROR("Failed to enable Master secure for SPORT0A\n");
   		return FAILED;
       }

       /* Make SPORT 0B to generate secure transactions */
       if(adi_spu_EnableMasterSecure(ghSpu, SPORT_5B_SPU, true) != ADI_SPU_SUCCESS)
       {
       	REPORT_ERROR("Failed to enable Master secure for SPORT0B\n");
   		return FAILED;
       }
       if(adi_spu_EnableMasterSecure(ghSpu, SPORT_6A_SPU, true) != ADI_SPU_SUCCESS)
          {
          	REPORT_ERROR("Failed to enable Master secure for SPORT0A\n");
      		return FAILED;
          }

          /* Make SPORT 0B to generate secure transactions */
          if(adi_spu_EnableMasterSecure(ghSpu, SPORT_6B_SPU, true) != ADI_SPU_SUCCESS)
          {
          	REPORT_ERROR("Failed to enable Master secure for SPORT0B\n");
      		return FAILED;
          }
          if(adi_spu_EnableMasterSecure(ghSpu, SPORT_7A_SPU, true) != ADI_SPU_SUCCESS)
             {
             	REPORT_ERROR("Failed to enable Master secure for SPORT0A\n");
         		return FAILED;
             }

             /* Make SPORT 0B to generate secure transactions */
             if(adi_spu_EnableMasterSecure(ghSpu, SPORT_7B_SPU, true) != ADI_SPU_SUCCESS)
             {
             	REPORT_ERROR("Failed to enable Master secure for SPORT0B\n");
         		return FAILED;
             }

    return SUCCESS;
}

void Write_TWI_8bit_Reg(unsigned char Reg_ID, unsigned char Tx_Data)
{
	devBuffer[0] = Reg_ID;
	devBuffer[1] = Tx_Data;
	adi_twi_Write(hTwiDevice, devBuffer, 2u, false);
}

uint8_t Read_TWI_8bit_Reg(unsigned char Reg_ID)
{
	ADI_TWI_RESULT eResult;
	uint8_t Rx_Data;

	/* write register address */
	devBuffer[0] = Reg_ID;
	eResult = adi_twi_Write(hTwiDevice, devBuffer, 1u, true);
	if(eResult!=ADI_TWI_SUCCESS)
	{
		//REPORT_ERROR("TWI write failed 0x%08X\n", eResult);
	}

	/* read register value */
	eResult = adi_twi_Read(hTwiDevice, &Rx_Data, 1u, false);
	if(eResult!=ADI_TWI_SUCCESS)
	{
		//REPORT_ERROR("TWI Read failed 0x%08X\n", eResult);
	}

	return Rx_Data;
}

static int32_t Init_TWI(void)
{
	ADI_TWI_RESULT eResult;

	eResult = adi_twi_Open(TWIDEVNUM, ADI_TWI_MASTER, &TwideviceMemory[0],
			   	ADI_TWI_MEMORY_SIZE, &hTwiDevice);
	if(eResult!=ADI_TWI_SUCCESS)
	{
		//REPORT_ERROR("TWI Open failed 0x%08X\n", eResult);
	}

	eResult = adi_twi_SetPrescale(hTwiDevice, PRESCALEVALUE);
	if(eResult!=ADI_TWI_SUCCESS)
	{
		//REPORT_ERROR("TWI Set Prescale failed 0x%08X\n", eResult);
	}

	eResult = adi_twi_SetBitRate(hTwiDevice, BITRATE);
	if(eResult!=ADI_TWI_SUCCESS)
	{
		//REPORT_ERROR("TWI Set Bitrate failed 0x%08X\n", eResult);
	}


	eResult = adi_twi_SetDutyCycle(hTwiDevice, DUTYCYCLE);
	if(eResult!=ADI_TWI_SUCCESS)
	{
		//REPORT_ERROR("TWI Set Duty cycle failed 0x%08X\n", eResult);
	}

	eResult = adi_twi_SetHardwareAddress(hTwiDevice, TARGETADDR);
	if(eResult!=ADI_TWI_SUCCESS)
	{
		//REPORT_ERROR("TWI Set Hw address failed 0x%08X\n", eResult);
	}

	return eResult;
}

static int32_t Stop_TWI(void)
{
	ADI_TWI_RESULT eResult;

	eResult = adi_twi_Close(hTwiDevice);
	CHECK_RESULT(eResult);

	return eResult;
}

/*****************************************************************************************************************************/

static int32_t ADAU_1962_init(void)
{
	int32_t i;
	ADAU_1962_Pllinit();
	for(i=0;i<28;i++)
	{
		/* write value */
		Write_TWI_8bit_Reg(Config_array_DAC[i].Reg_Add,Config_array_DAC[i].Value);
		Config_read_DAC[i]=Read_TWI_8bit_Reg(Config_array_DAC[i].Reg_Add);
		if(Config_array_DAC[i].Value!= Config_read_DAC[i])
		{
			DEBUG_INFORMATION("\n Configuring ADAU_1962 failed");
			return FAILED;
		}
	}

	return SUCCESS;
}

static int32_t ADAU_1962_Pllinit(void)
{
	int32_t status,delay1=0xffff;

	ADI_TWI_RESULT eResult;

   	eResult = adi_twi_SetHardwareAddress(hTwiDevice, TARGETADDR_1962);
	if(eResult!=ADI_TWI_SUCCESS)
	{
		//REPORT_ERROR("TWI Set Hw address failed 0x%08X\n", eResult);
	}

	Write_TWI_8bit_Reg(ADAU1962_PLL_CTL_CTRL0,0x01);
	while(delay1--)
	{
		asm("nop;");
	}

	Write_TWI_8bit_Reg(ADAU1962_PLL_CTL_CTRL0,0x05);

	delay1=0xffff;
	while(delay1--)
	{
		asm("nop;");
	}

	Write_TWI_8bit_Reg(ADAU1962_PLL_CTL_CTRL1,0x22);
	delay1=0xffff;
	while(delay1--)
	{
		asm("nop;");
	}
	status=Read_TWI_8bit_Reg(ADAU1962_PLL_CTL_CTRL1);
	while(!((status & 0x4)>>2)  )
	{
		status=Read_TWI_8bit_Reg(ADAU1962_PLL_CTL_CTRL1);
	}

	return eResult;
}




static int32_t ADAU_1979_init(void)
{
	int32_t i;

	ADAU_1979_Pllinit();

	for(i=0; i<16; i++)
	{
		Write_TWI_8bit_Reg(Config_array_ADC[i].Reg_Add,Config_array_ADC[i].Value);
		Config_read_ADC[i]=Read_TWI_8bit_Reg(Config_array_ADC[i].Reg_Add);
		if(Config_array_ADC[i].Value!= Config_read_ADC[i])
		{
			DEBUG_INFORMATION("\n Configuring ADAU_1979 failed");
			return FAILED;
		}
	}

	return SUCCESS;
}

static int32_t ADAU_1979_Pllinit(void)
{

	int32_t status,delay1=0xffff;

	ADI_TWI_RESULT eResult;

   	eResult = adi_twi_SetHardwareAddress(hTwiDevice, TARGETADDR_1979);
	if(eResult!=ADI_TWI_SUCCESS)
	{
		//REPORT_ERROR("TWI Set Hw address failed 0x%08X\n", eResult);
	}

   	Write_TWI_8bit_Reg(ADAU1979_REG_POWER,0x01);
	Write_TWI_8bit_Reg(ADAU1979_REG_PLL,0x03);
	status=Read_TWI_8bit_Reg(ADAU1979_REG_PLL);
	while(delay1--)
	{
		asm("nop;");
	}

	while(!((status & 0x80)>>7)  )
	{
		status=Read_TWI_8bit_Reg(ADAU1979_REG_PLL);
		asm("nop;");
	}

	return eResult;

}

//#define BYPASS_SS
int32_t nTempBuff[BLOCK_SIZE*NUM_CHANNELS];
void main(int32_t argc, char *argv[])
{
	/**
	 * Initialize managed drivers and/or services that have been added to
	 * the project.
	 * @return zero on success
	 */
	uint32_t Result=0, i, j;
	ADI_SS_MEM_BLOCK oConnectionMemBlk, *pConnectionMemBlk;
	ADI_SS_CONNECTION_CONFIG oConnConfig, *pConnConfig;
	ADI_SS_CONNECTION_RESULT eConnRet = ADI_SS_CONNECTION_FAILED;
	ADI_SS_CONNECTION_HANDLE hConnHandle;

	ADI_SS_MEM_BLOCK oCommMemBlk, *pCommMemBlk;
	ADI_SS_COMM_CONFIG oCommnConfig, *pCommnConfig;
	ADI_SS_COMM_RESULT eCommRet = ADI_SS_COMM_FAILED;
	ADI_SS_COMM_HANDLE hCommHandle;

	ADI_SS_RESULT eSSRes;
	SS_SMAP_SSN_INFO    *pSSnInfo;
	ADI_SS_COMM_PROPERTIES pCommProp;
	int32_t *pSportIn, *pSportOut,*pSportIn1,*pSportOut1,*pSportIn2,*pSportOut2,*pSportIn3,*pSportOut3,*pSportIn4;

	adi_initComponents();
	if(adi_pwr_audio_config() != 0u)
	    {
	        return 1u;
	    }
   /* SPU initialization */
	if (Result==0u)
	{
		Result=SPU_init();
	}

	/* Switch Configuration */
	//Switch_Configurator();
	PCG_init();
	/* SRU Configuration */
	SRU_Init();

	/* TWI Initialization */
	if (Result==0u)
	{
		//Result=Init_TWI();
	}

	/* ADAU1962 Initialization */
	if (Result==0u)
	{
		//Result=ADAU_1962_init();
	}

	/* ADAU1979 Initialization */
	if (Result==0u)
	{
		//Result=ADAU_1979_init();
	}

	if (Result==0u)
		{
			Result=Sport_Init();
		}
	/*******************************************************************************/
	/* SigmaStudio for SHARC (ADSP-SC5xx/ADSP-215xx) library integration */

	/* Connection component Initialization */
	pConnConfig = &oConnConfig;
	pConnConfig->eConnectionType = ADI_SS_CONNECTION_SPI;
	pConnConfig->nDevId = 0;
    pConnConfig->eProcID = PROCESSOR_SH0;

	pConnectionMemBlk = &oConnectionMemBlk;
	pConnectionMemBlk->nSize = ADI_SS_CONNECTION_MEMSIZE;
	pConnectionMemBlk->pMem = adi_ss_connection_mem;
	eConnRet = adi_ss_connection_Init(pConnectionMemBlk, pConnConfig, &hConnHandle);
	if(eConnRet != ADI_SS_CONNECTION_SUCCESS)
	{
        printf("\nConnection component initialization failed");
        exit(-1);
	}

	/* Communication component initialization*/
	pCommnConfig = &oCommnConfig;
	pCommnConfig->bCRCBypass = false;
	pCommnConfig->bFullPacketCRC = true;
	pCommnConfig->pfCommCmd4CallBack = (ADI_SS_COMM_CMD4_CB) adi_ss_comm_callback_cmd4;
	pCommnConfig->pfCommSMAPCallBack = (ADI_SS_COMM_SMAP_CB) adi_SMAP_Application_Callback;
	pCommnConfig->hConnectionHandle = hConnHandle;
	pCommnConfig->pMemSMap[PROCESSOR_SH0] = &oSMAPSharc0;
	pCommnConfig->pBkChnlInfo[0] = &oBkChannelInfoSharc0;

	pCommMemBlk = &oCommMemBlk;
	pCommMemBlk->nSize = ADI_SS_COMM_MEMSIZE;
	pCommMemBlk->pMem = adi_ss_commn_mem;
	eCommRet = adi_ss_comm_Init(pCommMemBlk, pCommnConfig, &hCommHandle);
	if(eCommRet != ADI_SS_COMM_SUCCESS)
	{
        printf("\nCommunication component initialization failed");
        exit(-1);
	}
    //memcpy(&oSMAPSharc0,adi_ss_smap_DiffDXESchematic_0,adi_ss_smap_DiffDXESchematic_0_size*4);
	memcpy(&oSMAPSharc0,adi_ss_smap_IC_1,adi_ss_smap_IC_1_size*4);
	/* Wait for SMAP to be received from host */
#if  0
	while(!nSMAPReceived)
	{

	}
#endif
	/* Populating Memory addresses of different blocks from SMAP */
	oSSnMemMap.nMemBlocks = 11;
	pSSnInfo = &oSMAPSharc0.oSSnInfo[0];
	for(i=0; i<oSSnMemMap.nMemBlocks; i++)
	{
		oSSnMemMap.pMemBlocks[i] = &pSSnInfo->oSSnBuff[i];
	}

	/* Create an instance of SSn */
	adi_ss_create( &hSSnHandle, &oSSnMemMap);
	if(hSSnHandle == NULL)
	{
		printf("\n SSn instance creation failed");
		exit(-1);
	}

	/* Provide SSn handle to communication component using the adi_ss_comm_SetProperties() API */
	pCommProp.haSSnHandle[PROCESSOR_SH0][0] = hSSnHandle;
	pCommProp.nNumProcBlocks = 1;
	pCommProp.nProcId = PROCESSOR_SH0;
	eCommRet = adi_ss_comm_SetProperties(hCommHandle,ADI_COMM_PROP_SSN_HANDLE,&pCommProp);
    if(eCommRet != ADI_SS_COMM_SUCCESS)
	{
		printf("\nError in Communication component");
		exit(-1);
	}

	/* Initialize the SSn instance */
	pSSnConfig = &oSSnConfig;
	pSSnConfig->hSSComm = hCommHandle;
	pSSnConfig->nBlockSize = BLOCK_SIZE ;
	pSSnConfig->nInChannels = 16;
	pSSnConfig->nOutChannels = 16;
	pSSnConfig->bSkipProcessOnCRCError = 0;
	pSSnConfig->bSkipInitialDownload = 1U;
	pSSnConfig->nInitNoWait = 1;
	pSSnConfig->eProcID = PROCESSOR_SH0;
	pSSnConfig->bClearUnusedOutput = 1;

   // memcpy(oSSnMemMap.pMemBlocks[1]->pMem,adi_ss_code_DiffDXESchematic_0,adi_ss_code_DiffDXESchematic_0_size*2);
   // memcpy(oSSnMemMap.pMemBlocks[5]->pMem,adi_ss_param_DiffDXESchematic_0,adi_ss_param_DiffDXESchematic_0_size*4);
	memcpy(oSSnMemMap.pMemBlocks[1]->pMem,adi_ss_code_IC_1,adi_ss_code_IC_1_size*2);
	memcpy(oSSnMemMap.pMemBlocks[5]->pMem,adi_ss_param_IC_1,adi_ss_param_IC_1_size*4);


	eSSRes =  adi_ss_init(hSSnHandle, pSSnConfig);
	if(eSSRes != ADI_SS_SUCCESS)
	{
		printf("\nSSn instance initialization failed");
		exit(-1);
	}

	pSSnProperties = &oSSnProperties;

	/* Initialize SigmaStudio I/O pointers */
	for(i=0; i<NUM_CHANNELS; i++)
	{
		pSSInBuff[i] = &aSSInOutBuff[i*BLOCK_SIZE];
		pSSOutBuff[i] = pSSInBuff[i];
	}

	/* Populating hardcoded values for readback */
	for(i=0; i<3; i++)
	{
		oBkChannelInfoSharc0.nAvgMIPS[i]=0.0;
		oBkChannelInfoSharc0.nPeakMIPS[i]=0.0;
		oBkChannelInfoSharc0.nVersionInfo=0x47000000;
	}

	/*******************************************************************************/

	/* SPORT Initialization */
	//if (Result==0u)
	//{
		//Result=Sport_Init();
	//}

	/* Close TWI */
	if (Result==0u)
	{
		Result=Stop_TWI();
	}

	while(1)
	{
#ifdef BYPASS_SS
		if(nDataAvail >= 1)
		{
			nDataAvail = 0;

			if(CallbackCount == 1)
			{
				pSportIn = &int_SP0ABuffer4[0];
				pSportOut = &int_SP0ABuffer1[0];
			}
			else if(CallbackCount == 2)
			{
				pSportIn = &int_SP0ABuffer5[0];
				pSportOut = &int_SP0ABuffer2[0];
				CallbackCount=0;
			}

		   for(i=0,j=0;i<BLOCK_SIZE*NUM_CHANNELS;i+=NUM_CHANNELS,j+=NUM_CHANNELS)
		   {
			   /*Copy ADC buffer to DAC buffer */
			   pSportOut[j]  = pSportIn[i];
			   pSportOut[j+4] = pSportIn[i];
			   pSportOut[j+1] = pSportIn[i+1];
			   pSportOut[j+5] = pSportIn[i+1];
			   pSportOut[j+2] = pSportIn[i+2];
			   pSportOut[j+6] = pSportIn[i+2];
			   pSportOut[j+3] = pSportIn[i+3];
			   pSportOut[j+7] = pSportIn[i+3];
		   }
		}
#else
		if(nDataAvail >= 1)
		{
			nDataAvail = 0;

			if(CallbackCount == 1)
			{
				pSportIn = &int_SP4ABuffer3[0];
				pSportOut = &int_SP0ABuffer1[0];
				pSportIn1 = &int_SP5ABuffer3[0];
		        pSportOut1 = &int_SP1ABuffer1[0];
				//pSportIn2 = &int_SP6ABuffer1[0];
		       // pSportOut2= &int_SP6ABuffer3[0];
				//pSportIn3 = &int_SP7ABuffer1[0];
				//pSportIn3 = &int_SP0ABuffer1[0];
		       // pSportOut3 = &int_SP7ABuffer3[0];
			}
			else if(CallbackCount == 2)
			{
				pSportIn = &int_SP4ABuffer4[0];
				pSportOut = &int_SP0ABuffer2[0];
				pSportIn1 = &int_SP5ABuffer4[0];
				pSportOut1 = &int_SP1ABuffer2[0];
				//pSportIn2 = &int_SP6ABuffer2[0];
		       // pSportOut2 = &int_SP6ABuffer4[0];
				//pSportIn3 = &int_SP7ABuffer2[0];
				//pSportIn4 = &int_SP0ABuffer2[0];
		        //pSportOut3 = &int_SP7ABuffer4[0];

				CallbackCount=0;
			}



            /* Copy data from first Input SPORT */
			 /* Copy data from first Input SPORT */
			            memcpy(nTempBuff, pSportIn, BLOCK_SIZE * (NUM_CHANNELS/2) * sizeof(int));

			            /* Copy data from second Input SPORT */
			             memcpy(nTempBuff+(1 * BLOCK_SIZE * NUM_CHANNELS/2),pSportIn1,BLOCK_SIZE * NUM_CHANNELS/2 * sizeof(int));

			            /* Fixed to float conversion and copy to SS input buffer */
			            for (j = 0; j < NUM_SOURCE_SPORT; j++)
			            {
			                /* For first Input SPORT Channels */
			                if (j == 0)
			                {
			                    for (i = 0; i < NUM_CHANNELS/2; i++)
			                    {
			                        CopyFix2Float((volatile uint32_t *)&nTempBuff[(j * BLOCK_SIZE * NUM_CHANNELS/2) + i],
			                                      NUM_CHANNELS/2,
			                                      pSSInBuff[(j * NUM_CHANNELS/2) + i], 1, BLOCK_SIZE, 0u);
			                    }
			                }

			                /* For second Input SPORT Channels */
			                if (j == 1)
			                {
			                    for (i = 0; i < NUM_CHANNELS/2; i++)
			                    {
			                        CopyFix2Float((volatile uint32_t *)&nTempBuff[(j * BLOCK_SIZE * NUM_CHANNELS/2) + i],
			                                      NUM_CHANNELS/2,
			                                      pSSInBuff[(j * NUM_CHANNELS/2) + i], 1, BLOCK_SIZE, 0u);
			                    }
			                }
			            }

			/* Call to the Schematic processing  */
			adi_ss_schematic_process(hSSnHandle,BLOCK_SIZE,(adi_ss_sample_t **)pSSInBuff,(adi_ss_sample_t **)pSSOutBuff,pSSnProperties);

#if 0			/* Float to fix conversion and copy back to SPORT buffer */
			for(i=0; i<NUM_CHANNELS; i++)
			{
				CopyFloat2Fix(pSSOutBuff[i], 1, (volatile uint32_t * )&pSportOut[i], NUM_CHANNELS, BLOCK_SIZE, 0u);
			}
			//for(i = 0; i < NUM_CHANNELS/2; i++) {
			    // 后8通道:SigmaStudio通道8-15 → SPORT1A
			   // CopyFloat2Fix(pSSOutBuff[i + 8], 1,(volatile uint32_t * )&pSportOut4[i], NUM_CHANNELS/2, BLOCK_SIZE, 0u);
			//}
#endif
#if 1

            /* Float to fix conversion and copy back to SPORT buffer */
            for (i = 0; i < 16; i++)
            {
                if (i < 8)
                {
                    /* For first Output SPORT Channels */
                    CopyFloat2Fix(pSSOutBuff[i], 1, (volatile uint32_t *)&pSportOut[i],
                                  8, BLOCK_SIZE, 0u);
                }
                else if (i < 16)
                {
                    /* For second Output SPORT Channels */
                    CopyFloat2Fix(pSSOutBuff[i], 1, (volatile uint32_t *)&pSportOut1[i],
                                  8, BLOCK_SIZE, 0u);
                }

                // {
                //     printf("\nCore1: Please check number of channel configuration for the output SPORT's \n");
                // }
            }
#endif
#if 0
			/* Overwrite */
			for(i=0,j=0;i<BLOCK_SIZE*NUM_CHANNELS;i+=NUM_CHANNELS,j+=NUM_CHANNELS)
			{
			   /*Copy ADC buffer to DAC buffer */
			   pSportOut[j]  = pSportIn[i];
			   pSportOut[j+4] = 0;
			   pSportOut[j+1] = pSportIn[i+1];
			   pSportOut[j+5] = 0;
			   pSportOut[j+2] = 0;
			   pSportOut[j+6] = 0;
			   pSportOut[j+3] = 0;
			   pSportOut[j+7] = 0;
			}
#endif

			if(nDataAvail >2)
			{
				printf("\n Input buffer overflow detected");
				exit(-1);
			}
		}
#endif
	}
}


void adi_SMAP_Application_Callback(ADI_SS_PROC_ID eCoreID)
{
	if(eCoreID==PROCESSOR_SH0)
	{
		nSMAPReceived = 1;
	}
}



void adi_ss_comm_callback_cmd4(uint32_t *pCommPayloadBuff, int32_t  nPayloadCount, ADI_SS_SSN_HANDLE hSSn)
{
	;
}

In this project, I used two ADSP-21565 chips. The setup is ADC input - DSP1 - DSP2 - DAC output. When the 21565 is not performing any audio processing, the audio data from the ADC can pass directly to the DAC, and the music plays normally. However, when I integrate the SigmaStudio schematic into the 21565, only waveforms at specific frequencies can be output normally—for example, sine waves at 500Hz, 1000Hz, and 1500Hz work fine, but sine waves at 800Hz or 1200Hz show chaotic behavior. This happens whether it's the sine wave input from the ADC or the built-in sine wave in SigmaStudio; after output through the DAC, the same issue occurs. I suspect the problem lies in SigmaStudio's BLOCK_SIZE configuration, because when I set BLOCK_SIZE to a multiple of 96, the 1kHz sine wave outputs normally, but other frequencies that are not multiples of 500Hz have noise. Of course, it could also be a memory allocation issue.

So when the 21565 is running at a 96kHz sampling rate, how should the block_size be configured to avoid buffer overflow? When I set the block_size to 192, the CCES compilation reports a memory overflow, but when set to 384, there is no error. Why is that?

My code is developed based on LibraryIntegration.

Thread Notes

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.