Post Go back to editing

About version control in SIGMA STUDIO PLUS

Thread Summary

The user inquired about version control support in SigmaStudioPlus for ADSP-21568 projects, specifically if .ssproj files are suitable for Git. The final answer clarifies that SigmaStudioPlus includes a built-in schematic version control feature accessible via Tools > Project Version Control, which is not related to external version control systems. The user should not manually edit the 'Versions' section to maintain GUI consistency.
AI Generated Content
Category: Software
Product Number: sigma studio

I would like to ask about version control support in SigmaStudioPlus.
Is there any feature in SigmaStudioPlus that corresponds to the Version Control function in the original SigmaStudio?
The processor used is an ADSP-21568.
wiki.analog.com/.../schematicversion

According to the comparison table in the link below, it is mentioned that .ssproj files contain module information in text format, which makes them suitable for version control.
Therefore, I am assuming that SigmaStudioPlus projects are intended to be managed by Git or similar version control tools.
Is this understanding correct?
wiki.analog.com/.../comparison

On the other hand, there seems to be no documentation describing how consistency with the GUI is maintained.
For example, is it safe to manually edit fields such as the “Versions” section shown below?


There is no information available on the web, so any guidance would be greatly appreciated.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.