Post Go back to editing

Issue with ExportCodeParam.exe in SigmaStudio Plus (v2.4.0)

Thread Summary

The user encountered an error while generating .c and .h files using ExportCodeParam.exe in SigmaStudio Plus v2.4.0. The solution is to use the command: "ExportCodeParam.exe" "SWC" "volume_ADSP2156x_1_SharcXICore_3" "DiffDXESchematic_3" "215xx". Differences in exported system files between SigmaStudio and SigmaStudio Plus are noted, and more details are available on the Microcontroller Mode Support page on the Analog Devices Wiki.
AI Generated Content
Category: Software
Product Number: adsp-21568
Software Version: Sigma Studio Plus 2.4.0

Dear Team,

While using ExportCodeParam.exe from the installation path of SigmaStudio Plus (v2.4.0):

   (C:\Analog Devices\SigmaStudioPlus-Rel2.4.0\Target\Utilities\ExportCodeParam)

  we encountered an error during the generation of .c and .h files using the Exported Files option. Please find the attached error screenshot for reference.

              

However, when following the same procedure in SigmaStudio, the .c and .h files were generated successfully without any issues.

Additionally, we observed differences between the exported system files generated by SigmaStudio and SigmaStudio Plus. Please refer to the attached snapshots for comparison.

  Please share the procedure for using the .exe application to generate files in SigmaStudio Plus.

Regards,
Sundaram

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.