hi guys
I run the default example LibIntegrationExample_Core1 of adsp21569 , and run the default example ADSP-21569 Processing Audio With Routers Example to connect with the target ,
the LibIntegrationExample_Core1 have open sport 4A 4B for data transfering, I noticed the sigmastudio plus can config the sport setting

I config it and download it , but it seem not work , is the source sport in the SS+ correspond with the receive sport in cces, sink sport in SS+ correspond with the transmit sport in cces ?