Post Go back to editing

ADSP-SC589-EZ and SigmaStudioPlus

Contains AI Generated Content
Category: Software

I am using CCES 3.0.2 and SigmaStudioPlus 2.3.0 with ADSP-SC589-EZ board.

I am facing three issues in SigmaStudioPlus 2.3.0.

1) The simple Gain module does not have the NumChannels option, very inconvenient. Any plans to change this?

2) Delay can switch between milliseconds and samples. The ms field has not the needed resolution to cover 1 sample. If a sample value is entered as input, and then the presentation is changed to milliseconds, and then changed back to samples again, the sample value is changed. This means that the delay setting is corrupted if the display mode is changed. 

The old SigmaStudio 4.7 did not have this issue. There, the ms resolution was enough to keep the sample value intact when changing the display from ms to samples and back again. There is no reason why SigmaStudioPlus should not behave in the same way.

3) The sampling rate is selectable up to 192kHz, but not higher than that. What is the reason? Is there any workaround available to allow 384kHz?

BN

Edit Notes

Reformulating the questions to improve the likelihood to get ANY answer, complete silence after 3 weeks of posting
[edited by: bnilsson at 4:07 PM (GMT -4) on 21 Jun 2025]

Thread Notes

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.