Post Go back to editing

First steps with SC589 MINI Evaluation: communication fails

Category: Software
Product Number: ADZS-SC589-MINI
Software Version: Sigma Studio+ v2.2.0

Dear community, 

I am currently checking out the SHARC SC589 (Mini evaluation board) with SigmaStudio (+). Unfortunately, I'm unable to download any program to the board (Starting with the Example Script). Sigma Studio always returns: 'Target verification could not be verified' after hitting the 'Link Compile Download' button. When turning Target verificiation off, it doesn't change anything. The board seems to be completely unaffected as it doesn't change it's output / doesn't output anything. Therefore must be something wrong with the communication, I guess.

I am using the same USBi interface as I have used several times with other ADAU-boards successfully. The jumper (JP1) is set to SPI-Boot.

Do you have any guide or idea what the problem could be? Should I use different software, are there any prerequisites that need to be done before using SigmaStudio with SC589 and furthermore, is there any specific guide/documentation for this board in combination with SigmaStudio?

I do appreciate any help or hint!

Best regards

Sebastian

Parents Reply Children