SigmaStudio+ version details:
I am using the Algorithm Designer to create some custom modules and I want to use a table to control a parameter.
I have created a parameter on the Parameter Definition tab and have created a corresponding variable on the variables tab which I have set as a Numeric Array.
Now the issue I am having is that if I change the size of the numeric array variable from the default 10, it doesn't seem to save properly in the .adprj file. So if I save the Algorithm Designer project, close it and reopen it again from file, the variable will have gone back to the default size of 10.