I have an application that I developed in SigmaStudio for the ADAU1467. At this point I have maxed out the instruction cycles and am considering moving to a 21489. The issue is that the application that uses the ADAU1467 interacts with the device through a sigmatcpserver that, in turn, uses the SPI interface to interact with the 1467. This give me interactive control over filters, volume controls etc. that I need for my application. The sigmatcpserver that I am using is some open source software written in python. I don't believe that CrossCore has TCPIP communication channel blocks in the same way that SigmaStudio does and I am fine with using an ICE1000 for programming but I definitely need fine-grained control by the application. Is there anyone that has any experience with a TCPIP/SPI 'bridge' for interfacing with the ADSP chips? Any tips would be much appreciated.
moved and updated the form
[edited by: GenevaCooper at 11:30 PM (GMT -4) on 24 Sep 2023]