Does the Sigmastudio plus support to custom algorithm for ADSP21489?
Only one selection is ADSP-SC5xx, but it can be used for ADSP-215xx, but if DSP is ADSP-21489 then can't find the custom algorithm item.
ADSP-21489
Production
The SHARC ADSP-21489 is one of two new members of the fourth generation of SHARC® Processors that now includes the ADSP-21483, ADSP-21486, ADSP-21487,...
Datasheet
ADSP-21489 on Analog.com
Does the Sigmastudio plus support to custom algorithm for ADSP21489?
Only one selection is ADSP-SC5xx, but it can be used for ADSP-215xx, but if DSP is ADSP-21489 then can't find the custom algorithm item.
Hi OJack;
Not an ADI staff.
You can create schematic for ADSP-21489 however the sigmastudio+ target library does not support SMAP
and downloading schematic thru USBi won't work. I suspect ADI release has been broken but correct me if I am wrong.
To create project for ADSP-21489, follow System Implementation [Analog Devices Wiki] to select platforms of 21489 or you could start with the example Tutorials and Examples [Analog Devices Wiki].
Yours
Totoro
No, Sigmastudio plus won't support to custom algorithm for ADSP21489. The algorithm designer support for ADSP-214xx will be available in next SS+ release expected early August 2023