Post Go back to editing

SigmaStudioPlus can not start

Category: Software
Product Number: EV-21569-SOM REV B
Software Version: SigmaStudioPlus rel2.0.0

I am using SigmaStudioPlus to import a previous SS project. After I imported with the XMLs successfully, I tried to open the Schematics inside. And my SigmaStudioPlus finally crashed and exited by itself. Then, when I try to reopen the SigmaStudioPlus, it will suspend at the following UI:

And I have tried to uninstall & reinstall SigmaStudioPlus, but it still can not start. Could you tell me why and how to solve it?

Parents
  • Hi, 
    do you have admin permission for the PC/Laptop? SigmaStudio needs admin permission to generate and keep temporary program data, so you can try as an administrator. 
    Also restart the PC and try again, If you are facing the same issue, please share the SS schematic file which you are facing this issue.

  • I am using the Laptop of the Company, and I have no admin permission. But I have tried to run it by selecting "Run as administrator" option, and it keeps suspending at the starting UI, too. I have ever started it up before, so I think I SHOULD also be able to run it at this stage, right? To make things more clear, I would like to paste the XMLs I imported that are exported from previous SS project as bellow:

Reply
  • I am using the Laptop of the Company, and I have no admin permission. But I have tried to run it by selecting "Run as administrator" option, and it keeps suspending at the starting UI, too. I have ever started it up before, so I think I SHOULD also be able to run it at this stage, right? To make things more clear, I would like to paste the XMLs I imported that are exported from previous SS project as bellow:

Children