I am using SigmaStudio Plus 2.0.0 to design schematic for ADSP 21562. In the schematic setting tab, the Input Channels combobox is non-tunable hence fixed to 8chs. How could I choose other setting like 32ch?
Best Regards!
Yao
ADSP-21489
Production
The SHARC ADSP-21489 is one of two new members of the fourth generation of SHARC® Processors that now includes the ADSP-21483, ADSP-21486, ADSP-21487,...
Datasheet
ADSP-21489 on Analog.com
I am using SigmaStudio Plus 2.0.0 to design schematic for ADSP 21562. In the schematic setting tab, the Input Channels combobox is non-tunable hence fixed to 8chs. How could I choose other setting like 32ch?
Best Regards!
Yao
Hi,
The default schematic within the processor has 8Ch input block, so the user not allowed to change number of input by default.
You need to remove the input module, which is present in the schematic project. Then you should be able to update the number of input channels. After setting the required number of input channels, you can insert the input block back to the schematic project.
Thanks.
Thank you! It is exactly the case.