when using exportCodeParam.exe , error occurs. exportCodeParam.exe "SWC" "ToneGen_Equalizer_Compressor_Block_2156x" "IC_1" "215xx"
when using exportCodeParam.exe , error occurs. exportCodeParam.exe "SWC" "ToneGen_Equalizer_Compressor_Block_2156x" "IC_1" "215xx"
Hi,
Please export the file with same name what you are using in the command exportCodeParam.exe "SWC" "ToneGen_Equalizer_Compressor_Block_2156x" "IC_1" "215xx".
Hi Sakthivel;
Where could I find exportCodeParam.exe for SigmaStudioPlus?
And Where does IC_1 argument come from? I found all exported file does not contains "IC_1" in the file name:
TDMLoopback_ADSP2156x_1.json
TDMLoopback_ADSP2156x_1.xml
TDMLoopback_ADSP2156x_1_NetList.xml
TDMLoopback_ADSP2156x_1_Target.xml
TDMLoopback_DiffDXESchematic_1.h
TDMLoopback_DiffDXESchematic_1.param
TDMLoopback_DiffDXESchematic_1_Defines.h
TDMLoopback_DiffDXESchematic_1_NumBytes.dat
TDMLoopback_DiffDXESchematic_1_PARAM.h
TDMLoopback_DiffDXESchematic_1_TxBuffer.dat
TDMLoopback_DiffDXESchematic_1_TxMetaBuffer.dat
And using exportCodeParam.exe from SS4S 4.7 does not work.
$ ./exportCodeParam.exe SWC TDMLoopback IC_1 215xx ERROR: Export Utility could not found SMAP or Code or Parameter sizes. Please check exported files Press ESC to stop $ ./exportCodeParam.exe SWC TDMLoopback ADSP2156x_1 215xx ERROR: Export Utility could not found SMAP or Code or Parameter sizes. Please check exported files Press ESC to stop
Using DiffDXESchematic_1 instead of IC_1, exportcodeparam.exe generate an empty file.
$ ./exportCodeParam.exe SWC TDMLoopback DiffDXESchematic_1 215xx Creating ./adi_ss_ssn_export_TDMLoopback_DiffDXESchematic_1.c file Program terminated successfully
Yours
Totoro
Hey Sakthivel P ,
I have the same issue here. When i generate the .c and .h File, I get an empty .h and .c file, containing only the imports.
Exported Files:

Then i call
.\ExportCodeParam.exe "SWC" "Exploration_SHARC_ADSP2156x_1_SharcXICore_3" "DiffDXESchematic_3" "215xx" Creating ./adi_ss_ssn_export_Exploration_SHARC_ADSP2156x_1_SharcXICore_3_DiffDXESchematic_3.c file Program terminated successfully
But the files are empy except for the includes. What do i need to modify to generate the files correctly?
.c-File
/* 09.12.2025 13:05:18 */ #include "adi_ss_common.h" #include "adi_ss_ssn_export_Exploration_SHARC_ADSP2156x_1_SharcXICore_3_DiffDXESchematic_3.h"
.h-File
/* 09.12.2025 13:05:18 */ #include <adi_types.h>
Best regards,
Eric
Please share the schematic to simulate this error.
Which version of SigmaStudio+ you are using?
Hi Sakthivel P ,
thanks for the fast reply. I am using:
- SigmaStudio+ v2.4
- CCES v2.12.1
Here is my DXE and the schematic file. Exploration_SHARC.zip
Best regards,
Eric
Hi,
I didn't see any issue with following SS+ schematic source file export command. Please refer this link for more details.
Microcontroller Mode Support [Analog Devices Wiki]
5415.Exploration_SHARC.zip
Hi,
Please use the export utility from SS+ installation folder, this command may work for you,
"C:\Analog Devices\SigmaStudioPlus-Rel2.4.0\Target\Utilities\ExportCodeParam\ExportCodeParam.exe" "SWC" "TDMLoopback" "DiffDXESchematic_1" "215xx"
Hi Sakthivel P ,
I see that in you header file everything is okay. But I can't generate it on my own. When I call it like you descibed (call below), it works but the files are still empty.
'C:\Analog Devices\SigmaStudioPlus-Rel2.4.0\Target\Utilities\ExportCodeParam\ExportCodeParam.exe' "SWC" "Exploration_SHARC_ADSP2156x_1_SharcXICore_3" "DiffDXESchematic_3" "215xx" Creating ./adi_ss_ssn_export_Exploration_SHARC_ADSP2156x_1_SharcXICore_3_DiffDXESchematic_3.c file Program terminated successfully
What could be the reason for the empty files?
Best regards,
Eric
is there a exported file "Exploration_SHARC_ADSP2156x_1_SharcXICore_3_DiffDXESchematic_3.h" in schematic export files?
If Yes it should have proper data like this "ADI_REG_TYPE SMAP_SH0_DIFFDXESCHEMATIC_3_Data[SMAP_SH0_SIZE_DIFFDXESCHEMATIC_3] = {".
Since your export files have Core name, I will try it once from my end.
May I know you need this big file name?
Some times windows path issue may lead to this issue.
Hi Sakthivel P ,
yes there is the "Exploration_SHARC_ADSP2156x_1_SharcXICore_3_DiffDXESchematic_3.h" with a lot of content in it. Regarding the Filename, i just exported the file without any changes in SigmaStudio+. The Projectname is simply "Exploration_SHARC" and SigmaStudio+ appends the filename. I remove the settings to append the name in SigmaStudio+ and check if this fixes the issue.
Best regards,
Eric
Hi Sakthivel P ,
it was the filename or the appendix with core/processor name. When i remove to append the file with core and processor name it works. Thanks a lot for your support.
Best regards,
Eric
Hi Sakthivel P ,
it was the filename or the appendix with core/processor name. When i remove to append the file with core and processor name it works. Thanks a lot for your support.
Best regards,
Eric