ADSP-21569
Recommended for New Designs
Reaching speeds of up to 1 GHz, the ADSP-2156x processors are members of the SHARC® family of products. The ADSP-2156x processor is based on the SHARC...
Datasheet
ADSP-21569 on Analog.com
I have a ev21569-som+ ev-somcrr-ezkit board and it connect a ADZS-AD2428MIN over J10. In addition, the ADZS-AD2428MINI connect to a A2B EVAL-AD2428WB1BZ(this board has two microphones) over A2B bus as well. I would like to use SigmaStudio to create a audio route to allow me capture the 2PDM microphones from 21569. do you have a SigmaStudio dspprog likes adi_a2b_3NodeSampleDemoConfig.dspproj? Or if you have any guide to show me how to use SigmaStudio for ev21569-som+ ev-somcrr-ezkit board that also great.
thanks,
Kylin
Hi,
Could you please share the Signal flow details of 2 PDM Mic data on 21569?
Thanks.
Hi,
Could you please share the Signal flow details of 2 PDM Mic data on 21569?
Thanks.
The 2 PDM mics on the EVAL-AD2428WB1BZ. This EVAL-AD2428WB1BZ board is a a2b slave and it connect the ADZS-AD2428MINI over A2B bus. Then ADZS-AD2428MINI connect to ev-somscrr-ezkit by J10. I would like to create a route to capture the 2 mics data from 21569 by TDM inteface. Do you have that example?
1) You can add source and sink for A2B I/O using SigmaStudio schematic "IC1 -ADSP-SC5xx Control --> Faramework config" window.
Add source for input to 21569 and add Sink for output from 21569. Also chose the SPORT for configure the data pin.
2) In SRU of target application make sure whether Bit clock and LR clock is assigned to right DAI pins connected to A2B main/sub.
somehow, I cannot ADSP-21569. Do you know which package should I install? I have installed the SigmaStudioForSHARC-SH-Rel2.2.0
Hi Sakthivel,
Would you please let me know which version of sigmastudio I have to install? I did not see the 21569 from sigmastudio v4.7. Could you please list all the relate package here?
thanks,
Alan
Hi,
Please contact your regional Analog Devices representatives for more details.
Thanks