I and using ADSP-SC589 EZ board, and the ICE-1000 debug interface.
I am migrating from CCES 2.10.0 to 2.11.1.
I have built the SS_App framework to use together with SigmaStudio 4.7 in CCES 2.11.1.
In order to download the SigmaStudio project to the framework, you of course need to run the SS_App on the EZ board first as a "debug" session from CCES.
However, I get the following error from CCES:
assertion pAppArmCoreInfo->hssFWHandle != NULL failed
I have installed CCES 2.11.1 ONLY, on top of previous CCES versions and SigmaStudio for SHARC 4.5.
Should I reinstall SigmaStudio for SHARC?