Post Go back to editing

Is there a linux driver for the ADSP-21489?

Category: Software

Hello,

we currently use an ADAU1452 in our products. Our SOM runs on Linux 4.1.15. and we are very happy of this solution.

Our acousticians work with SIGMA Studio.

The driver had to addapt existing drivers to have this solution. But It's working well for while.


We would like to see if there is a driver or a driver base if we were to switch to the Sharc DSP (a SIGMAStudio compatible version).

I can't find anything anywhere?

Would you have a solution or a track to follow?

Best Regards

JB

Parents Reply
  • Thanks for the support.
    This the current questions we have:
     - LDR: Is the source code of the LDR is available somewhere ? (ss_app_sh369) for exemple to understand what is the scope of it and what must be done in the LDR and what can be set in the dspproj ?
     - Is the LDR selected into sigmaStudio is exported into the xml file, so It could be included into the bin file (and upload by our linux through SPI) like we did  with the ADAU ?
     - Is it inside the LDR code that we should handle the SPI communication between our Linux and the SigmaStudio boxes (eg changing the volume etc...)
    Best Regards
Children