Post Go back to editing

Sigma Studio for Sharc I/O

Category: Software
Product Number: SC5xx / 215xx

In Sigma Studio for Sharc the I/O seems very limited. I want to use a device with 8 SPORTS but it appears that only one input block is supported.

Am I missing something here or do people not really use Sigma Studio on the larger DSP parts?

Ian.

Parents
  • Hi Ian,


    May I know which SHARC DSP you are using?
    May I know which version of SigmaStudio for SHARC and SigmaStudio you are using?
    Also may I know you project details?

    The SigmaStudio for SHARC framework will support up to 8 SPORT which also have 2 half SPORT  each to receive/transmit data independently. The SigmaStudio schematic needs to  be configured for number of input/output channels, SPORT configuration and DAI Pin's to SPORT etc.  

    Please refer the documents available in SigmaStudio for SHARC installation folder, for example if you are using SigmaStudio for SHARC 4.7.0, then refer the path

    C:\Analog Devices\SoftwareModules\SigmaStudioForSHARC-SH-Rel4.7.0\Docs.

    Thanks.

Reply
  • Hi Ian,


    May I know which SHARC DSP you are using?
    May I know which version of SigmaStudio for SHARC and SigmaStudio you are using?
    Also may I know you project details?

    The SigmaStudio for SHARC framework will support up to 8 SPORT which also have 2 half SPORT  each to receive/transmit data independently. The SigmaStudio schematic needs to  be configured for number of input/output channels, SPORT configuration and DAI Pin's to SPORT etc.  

    Please refer the documents available in SigmaStudio for SHARC installation folder, for example if you are using SigmaStudio for SHARC 4.7.0, then refer the path

    C:\Analog Devices\SoftwareModules\SigmaStudioForSHARC-SH-Rel4.7.0\Docs.

    Thanks.

Children