Post Go back to editing

add more SPORT to ucDemo for SC589 has run out of memory on L2 memory.

Hi,

We using Sigmastudio 4.5 , Sigmastudio 4.5  for sharc and crosscore 2.9.4 on a sharc ADSP SC589.

When we add more sports to the ucDemo for SC589, we run out of memory on L2 memory.

We need 7 sports.

We had already try to change the following line in the .ld file.

/* ARM Core 0 L2 RAM, uncached */
/* MEM_L2_UNCACHED : ORIGIN = 0x20084000, LENGTH = 28K */
MEM_L2_UNCACHED : ORIGIN = 0x20084000, LENGTH = 76K /* max 77Kb */

/* ARM Core 0 L2 RAM, cached */
/* MEM_L2_CACHED : ORIGIN = 0x2008B000, LENGTH = 84K */
MEM_L2_CACHED : ORIGIN = 0x20097000, LENGTH = 32K /* max 35Kb */

After these changes we had the following overflow message.

..... `.ss_text' will not fit in region `MEM_L2_CACHED'
region `MEM_L2_CACHED' overflowed by 32684 bytes

What we need to change so that everything fits in the L2 memory.

Regards