Basic volume control on ADSPSC589 ez board.

I've attached a sample schematic from the example folder in sigmastudio which used to control volume and mute. In the schematic, there are 4 RCA inputs, 2 s/pdif inputs and 6 RCA outputs. I've used demo DXE (CCES) for ADSPSC589 given in the example folder of software module.

I have 1 RCA mic as input and 1 RCA speaker as output.

Can someone tell me how the processor knows which pins are input and which pins are output? That is, how and where to assign these pins as input and output. I've searched in manual but i couldn't find it. 

My second question is, if i want to use just 1 input and output how do i assign it in the code?

New here, kindly help. Thank you.

 

Parents
  • Hi,

    The default framework is considering, RCA output port is J16 for 8 channels output  and RCA input port is J6 for 4 channels input. For any change in channel configuration requires framework modifications. If you want to modify the framework, you need to understand the default framework code flow by running demo application in CCES debug mode. You can put break points in CCES debug mode, so you can understand the code flow.

    Thanks.

Reply
  • Hi,

    The default framework is considering, RCA output port is J16 for 8 channels output  and RCA input port is J6 for 4 channels input. For any change in channel configuration requires framework modifications. If you want to modify the framework, you need to understand the default framework code flow by running demo application in CCES debug mode. You can put break points in CCES debug mode, so you can understand the code flow.

    Thanks.

Children