Connecting ADSP-21489 EZ-KIT with SigmaStudio for SHARC

Hello,

I am having hard time with connecting SigmaStudio for Sharc with the ADSP-21489 EZ-KIT. The PC properly recognized the kit once USB was plugged it. However when I dragged the USBi block in SigmaStudio on the schematic it stayed red indicating the connection is not made.

I did follow the SigmaStudio Users Guide and configured all jumpers on the eval kit including the boot switch (SW4) to position 0 .

The kit uses ADZS-SADA2 board to interface between the kit (via 2 14pin headers) and the USB on PC.