I think the FAQ below is for SigmaStudioForSharc 2.2.0.
What do I want to know about SigmaStduioForSharc 4.7.0 and ADSP-21569? Can you tell me?
Edit
[edited by: nandar at 4:10 AM (GMT -4) on 14 Jul 2022]
ADSP-21569
Recommended for New Designs
Reaching speeds of up to 1 GHz, the ADSP-2156x processors are members of the SHARC® family of products. The ADSP-2156x processor is based on the SHARC...
Datasheet
ADSP-21569 on Analog.com
I think the FAQ below is for SigmaStudioForSharc 2.2.0.
What do I want to know about SigmaStduioForSharc 4.7.0 and ADSP-21569? Can you tell me?
Hi Der,
We have demoUc example with in the SigmaStudio for SHARC installation folder which uses generated schematic files with the target supplication.
You can refer the "AE_42_SS4G_QuickStartGuide.pdf" section "6.1 Loader file Flashing and Generation".
Thanks.
Dear Sakthivel P,
Is there a way to bypass the Framework?
If so, could you please provide an example code?
Your demoUc example codes all use the Framework...
Thank you
Regards
Hi,
you may look into the Library integration examples,
"C:\Analog Devices\SoftwareModules\SigmaStudioForSHARC-SH-Rel4.x.x\Target\Examples\LibraryIntegration"
Thanks.
Hi,
Thanks for your response,
I have already generated a .ldr file for an ADSP-21565 using SPI for loading the schematic, however it is not relevant when embedding the schematic within the loader.
In this case, LibraryIntegration doesn't help...
Regards
In lib integration you may need to copy the SAMP, code and parameters to the corresponding memory sections by referring the demouC example. Also you need to remove the "SMAP" download indefinite wait while loop. You cant directly use the example for schematic code.
In lib integration you may need to copy the SAMP, code and parameters to the corresponding memory sections by referring the demouC example. Also you need to remove the "SMAP" download indefinite wait while loop. You cant directly use the example for schematic code.