Hi,
I cannot program the evaluation board with Sigma Studio,
If I put 192KHZ in sampling frequency, on the other hand, it works, if I put 48KHZ.
Please explain to me how to make it work at 192KHZ?
Best regards,
Jean-pierre
Hi,
I cannot program the evaluation board with Sigma Studio,
If I put 192KHZ in sampling frequency, on the other hand, it works, if I put 48KHZ.
Please explain to me how to make it work at 192KHZ?
Best regards,
Jean-pierre
Hi,
The ADSP-21489 application is running at 48KHz sample rate by default, so you need to modify the application and regenerate LDR file for 192KHz.
If you are using SigmaStudioForSHARC-SH-Rel2.2.0 the CCES application project available in following path,
C:\Analog Devices\SoftwareModules\SigmaStudioForSHARC-SH-Rel2.2.0\Target\Demo\ADSP-21489
Just try changing compiler preprocessor in project settings as APP_SAMPLING_RATE=SAMPLING_RATE_192K and rebuild application to generate LDR file.
The regenerated LDR file can be used in SigmaStudio for running 192KHz processing.
Thanks,
Sakthivel
Ok,
Thanks.