Post Go back to editing

Secure boot in SC589 SAM board

Category: Software
Product Number: ADSP-SC589
Software Version: Cces 2.12.0

Hi,

I'm using SC589 SAM BOARD for my Project.Im facing a pbm in SPI flash boot.

I'm intended to use for secure booting.Im just following the EE366 but Simple LED Flash boot itself is not working.

- 1. First, I have modified led_blink as per SAM board which I got from SECURE Boot example of SC589 application note And it's working for me in debug mode. But in booting it's not working.

Ldr generation: Driver file added from SAM BSP, init file not included,Jumper 1&2 connected, SPI flash,bin,01.

Please give a solution for this.

2. Is sc589 mini supports secure boot? 

Thanks