Hi all,
I'm using the SC-589 on some custom hardware, with the bare metal framework. The hardware is organised such that there are two ADCs (both the same device, same settings), and I would like to feed each on into its own SHARC core for processing. ADC1 and SHARC core 1 are working fine using elements of the bare metal framework with custom initialisation code for the ADC. There is not audio out for the application, so I'm calculating the RMS of each channel and feeding this out on the UART once per second. As per the bare metal framework, I'm using I2S data into SPORT0 on SHARC core 1.
For SHARC core 2, the code functionality requirement is identical, the only changes are that SPORT 4, connected via DAI1 is used instead of SPORT0 on DAI0.
The code for SHARC core 1 has been duplicated for core 2, with the exceptions of:
- Changes to the SRU to connect the relevant DAI1 pins to SPORT4.
- Use of DMA11 interrupt for SPORT4B data reception
- Using a different TPU interrupt for the audio callback handler.
Whilst the code on SHARC core 1 works fine in terms of representative RMS values visible on the serial port, the values from the channels on SHARC core 2 are always 0. I've traced all the core 2 framework code through - both the dma handler and audio callback handler are working properly (checked with toggling pins on callback), and no samples are being dropped. Following the code back, and inserting known values into the buffers, it seems the issue is with the start of the dma routine - this seems to pull in only 0's to the input channels buffer:
// Artificially fill buffers:
for (i = 0; i < AUDIO_CHANNELS * AUDIO_BLOCK_SIZE; i++) {
ADC2_audiochannels_in[i] = 1;
}
// This is where we're getting stuck - sport4_dma_rx_0_buffer or sport4_dma_rx_1_buffer seems to be pulling in 0's
if ( (uint32_t)sport_dma_cfg->dma_descriptor_rx_0_list.Next_Desc !=
(*sport_dma_cfg->pREG_DMA_RX_DSCPTR_NXT)
) {
audioflow_float_to_fixed(ADC2_audiochannels_out, sport4_dma_tx_0_buffer, AUDIO_CHANNELS * AUDIO_BLOCK_SIZE);
audioflow_fixed_to_float(sport4_dma_rx_0_buffer, ADC2_audiochannels_in, AUDIO_CHANNELS * AUDIO_BLOCK_SIZE);
}
else
{
audioflow_float_to_fixed(ADC2_audiochannels_out, sport4_dma_tx_1_buffer, AUDIO_CHANNELS * AUDIO_BLOCK_SIZE);
audioflow_fixed_to_float(sport4_dma_rx_1_buffer, ADC2_audiochannels_in, AUDIO_CHANNELS * AUDIO_BLOCK_SIZE);
}
Artificially filling the buffers with known values after this point results in the RMS value jumping as expected.
So it would seem that the issue would be to do with the SRU, however I've double checked this with the graphical Signal Routing Unit configuration, and using the code below:
// Set up DAI pins as inputs and outputs for ADC 1
SRU(LOW, DAI0_PBEN16_I); // ADC1 BCLK is an input
SRU(LOW, DAI0_PBEN17_I); // ADC1 DAT is an input
SRU(LOW, DAI0_PBEN18_I); // ADC1 WS Out is an input
// Route BCLK and FS to SPORT 0 (which connects to DAI0)
SRU(DAI0_PB16_O, SPT0_ACLK_I); // route ADC1 BCLK pin to SPORT0A clock input
SRU(DAI0_PB16_O, SPT0_BCLK_I); // route ADC1 BCLK pin to SPORT0B clock input
SRU(DAI0_PB18_O, SPT0_AFS_I); // route ADC1 FS pin to SPORT0A frame sync
SRU(DAI0_PB18_O, SPT0_BFS_I); // route ADC1 FS pin to SPORT0B frame sync
// Route data signals
SRU(DAI0_PB17_O, SPT0_BD0_I); // route ADC1 SDATA Out pin to SPORT0B-D0 input
// SRU(HIGH, DAI0_PBEN01_I); // Loopback BCLK is an output
// SRU(HIGH, DAI0_PBEN02_I); // Loopback DAT is an output
// SRU(HIGH, DAI0_PBEN03_I); // Loopback WS Out is an output
// Route out to exposed pads for debug
// SRU(DAI0_PB16_O, DAI0_PB01_I);
// SRU(DAI0_PB17_O, DAI0_PB02_I);
// SRU(DAI0_PB18_O, DAI0_PB03_I);
// Set up DAI pins as inputs and outputs for ADC 2
SRU2(LOW, DAI1_PBEN16_I); // ADC2 BCLK is an input
SRU2(LOW, DAI1_PBEN17_I); // ADC2 DAT is an input
SRU2(LOW, DAI1_PBEN18_I); // ADC2 WS Out is an input
// Route BCLK and FS to SPORT 4 (which connects to DAI1)
SRU2(DAI1_PB16_O, SPT4_ACLK_I); // route ADC2 BCLK pin to SPORT4A clock input
SRU2(DAI1_PB16_O, SPT4_BCLK_I); // route ADC2 BCLK pin to SPORT4B clock input
SRU2(DAI1_PB18_O, SPT4_AFS_I); // route ADC2 FS pin to SPORT4A frame sync
SRU2(DAI1_PB18_O, SPT4_BFS_I); // route ADC2 FS pin to SPORT4B frame sync
// Route data signals
SRU2(DAI1_PB17_O, SPT4_BD0_I); // route ADC2 SDATA Out pin to SPORT4B-D0 input
// SRU2(HIGH, DAI1_PBEN01_I); // Loopback BCLK is an output
// SRU2(HIGH, DAI1_PBEN02_I); // Loopback DAT is an output
// SRU2(HIGH, DAI1_PBEN03_I); // Loopback WS Out is an output
// Route out to exposed pads for debug
// SRU2(DAI1_PB16_O, DAI1_PB01_I);
// SRU2(DAI1_PB17_O, DAI1_PB02_I);
// SRU2(DAI1_PB18_O, DAI1_PB03_I);
Scoping test points show all the correct I2S signals are present on the right pins, and I can route the I2S data back out onto a spare test point on another DAI1 pin, which would seem to indicate the routing works, so I'm at a bit of a loss as to where the issue is. Any insight would be greatly appreciated!