I am sure I am missing something obvious but it is escaping me at the moment. I have a CCES project based off the bare metal example that has all the required fixes for the SC589-Mini HW 2.1 and it works perfectly fin in debug and release when uploaded using the ICE-1000. I have the bootloader installed in flash and it also works fine and I am able to upload my ldr file. However on reboot I get two yellow flashes and then the fault light turns red immediately after. I assume something in my project setup like memory allocation may be at fault. I have done the obvious settings for the ldr file generation but also may have missed something.
I will keep plugging away at it but any help or useful directions for investigation would be appreciated.