Hi,
I have the SAM audio board and can add the faust volume example from the link below and it builds and runs perfectly.
https://github.com/moforte/sam-faust/tree/master/faust-examples/volume/volume-sam
I have seen similar issues for example
but if i compile the example using the online editor (https://fausteditor.grame.fr/) i get many errors on the build process on CCES.
in previous help version 2.6.1 of faust has been referred too but i can't find that on the repository so i have installed 2.60.3 for win64 (github.com/.../releases).
but i need some help on how to use it on windows.
The documentation pdf 'faust2sam Integration with the SHARC Audio Module Platform' section 1.4 it states that 'Currently, Faust is easily compiled and run on Mac/OS X machines and Linux machines. This document describes how to download, compile and
install Faust on a Mac/OS X machine'
so how do i use the windows version ?
i can see the 'faust.exe' and have listed the extensive help file but need some advice on how to use to compile a .dsp file to the files to drop into my CCES project.
Many thanks