The setup is the template CrossCore Embedded (2.11.1) SHARC Bare Metal framework project with no audio FIN, no Faust, and 1 SHARC core.
I have debugged through two issues: Setting up the ADAU1761 and looking for the multicore_data->sharc_core1_processing_audio flag set to true.
Both required a timeout while loop.
After this, however, it does not appear that the DMA is working, because the framework's process audio callback function within the SHARC core 1 code is not called.
Is there a correct / updated DMA configuration that is not present in the SHARC Bare Metal Release 2.1.2 framework?
Also, is there a beta for the next release of the framework?
Thanks,
Chris
Edit Notes
Type error[edited by: chlander73 at 11:52 PM (GMT -4) on 11 Sep 2023]